ZHCSJR9A May 2019 – November 2019 AMC1035-Q1
PRODUCTION DATA.
To decouple the power supply, place a 0.1-µF capacitor as close to the VDD pin of the AMC1035-Q1 as possible, as shown in Figure 48, followed by an additional capacitor in the range of 1 µF to 10 µF.
Figure 48. Decoupling the AMC1035-Q1 Safety considerations or high common-mode voltage levels can require the AMC1035-Q1 to be galvanically isolated from other parts of the system. Figure 49 shows an example of a circuit that uses the ISO7721-Q1 to isolate the signal path and the SN6501-Q1 and a transformer are used to generate the required isolated power.
Figure 49. Galvanic Isolation of the AMC1035-Q1