TIDT353 September 2023
Output voltage ripple is shown in the following figures.
In the following waveforms, channel 1 in dark blue is load current; channel 2 in light blue is input voltage; channel 3 in purple is AC portion of output voltage; channel 4 in green is the primary current.