TIDT321 January 2023
Switching behavior is shown in the following figures.
The waveform in Figure 3-1 was created using the following conditions: input voltage = 630 VDC; output
power = full load.
Figure 3-1 Switch NodeThe waveform in Figure 3-2 was created using the following conditions: input voltage = 330 VDC; output
power = full load.
Figure 3-2 Switch Node