Figure 2-1 and Table 2-1 describe package symbolization and the device revision code.
Figure 2-1 Package Symbolization
Table 2-1 Revision Identification
| Device Revision
Code |
Silicon Revision |
| B |
PG1.1 |
The die markings do not indicate the silicon
revision. However, customers can determine the silicon revision by one of the following
methods:
- TI provided software functions in chipinfo.c:
- HwRevision_t ChipInfo_GetHwRevision( void )
- Returns: chip HW revision
- HWREV_1_1 is returned for CC2651R3SIPA revision B.
- SmartRF™ Studio:
Figure 2-2 Device Identification with
SmartRF™ Studio
- Package label:
- The die revision name is shown on the tape and reel label as shown
in the example label in Figure 2-3.
- Entry (2P) lists the revision.
Figure 2-3 Sample Product Shipping Label for
the CC2651R3SIPA Device