SWRZ119A February 2022 – October 2026 CC1311R3
I2S bus faults are not reported
As an example; The TI-provided SPI driver SPICC26X2DMA.c will ensure that the flash memory is kept accessible also in Idle power mode if the transmit buffer address starts with 0x0 to ensure no bus faults occur. A similar approach needs to be taken if writing a peripheral driver utilizing I2S.