SWRU529C May 2017 – April 2020
When this display tab is selected, the chirp/frame parameters are taken from the actual configuration that was sent to the device and displayed (see Figure 18). In the case of advanced configuration, the values for the different subframes are shown separated by commas for each of the fields.
Figure 18. Display Parameters - Chirp/Frame