SWRA749 September 2022
This section provides information on how to configure the CC2564 device for the Bluetooth Low Energy (BLE) SIG RF PHY Testing.
The DUT is the CC2564 dual-mode Bluetooth device (possibly interfaced with host MPU/CPU). The Upper Tester is the PC which communicates with the DUT by sending HCI commands using UART 8-N-1 serial protocol. The DUT is also connected to the lower tester which is the Bluetooth tester (such as CBT Tester) via a U.FL/SMA connector.
Figure 7-1 Bluetooth SIG Core V4.0