SWRA725 November   2021 AWR2944 , IWR2944

 

  1.   Trademarks
  2. 1Introduction
  3. 2Crossing Interference
    1. 2.1 Performance Analysis for Crossing Interference
  4. 3Localization and Mitigation on the Hardware Accelerator (HWA)
    1. 3.1 Interference Statistics
    2. 3.2 Localization Module
    3. 3.3 Mitigation
  5. 4Summary
  6. 5References

Interference Statistics

Two kinds of statistics are computed on the ADC data [2]. These are:

  • The sum of absolute values of the adc data, a b s S u m =   i =   1 N x i where xi corresponds to the adc samples in the chirp.
  • The sum of the first difference of adc data, d i f f A b s S u m   =   i =   2 N x i - x i - 1 ,   .

These are then scaled down to generate means, and then scaled up to generate two thresholds (AbsThreshold and AbsDiffThreshold).

GUID-20211104-SS0I-J6P4-0BW7-XJKSGLNRDVKC-low.png
The abs-diff filters suppress the low-frequency tone and help make the glitch more visible.
Figure 3-3 Detecting Outliers Using Abs and Abs-diff Filters

The advantage of calculating the first difference is that it suppresses low-frequency reflections like the bumper reflection or the antenna coupling effect, allowing weaker glitches to be easily found.