While using the monitoring features,
the user must make sure the following conditions are met:
- Feedback channels are used for TX
SNR Monitoring- therefore, must not be used for data reception.
- One must make sure that both the
feedback channels have external 100Ω differential termination.
- There is no such requirement for
the RX channels.
- SNR Monitoring band must be
selected such that the band is signal free and must not contain any
external blockers. Improper band selection or signal leakage into
monitoring band can trigger false alarms.