SPRZ455G December 2020 – June 2026 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
PCIe: MMA Unsupported Request (UR) or Configuration Request Retry Status (CRS) in Configuration Completion Response Packets Results in External Abort
When the PCIe Root Port (RP) is enumerating a PCIe multi-function End Point (EP) device or a PCIe switch, the EP may respond with an Unsupported Request (UR) or a Configuration Request Retry Status (CRS) to a configuration read from the RP. The UR response is returned when the RP tries to access a Bus Device Function (BDF) resource that is non-existent in the EP. This type of configuration access and the UR response is expected during the enumeration process. The UR and the CRS response from the EP results in a bus error in the PCIe RP which causes a data abort to the CPU.
One of the following workarounds can be used: