SPRZ455G December 2020 – June 2026 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
PCIe: The 2-L SerDes PCIe Reference Clock Output can exceed the 5.0 GT/s Data Rate RMS jitter limit
When operating the 2-L SerDes PCIe Reference Clock in Output mode, the RMS jitter of the clock may exceed the PCIe specification limit for the 5.0 GT/s Data Rate.
Option 1:
Configure the Reference Clock output in Derived Refclk mode (as opposed to Received Refclk mode) and program the PLL configuration registers as follows:
Internal SSC mode requires no PLL configuration change.
For No SSC mode, the following registers should be written to change the PLL configuration:
Option 2:
Do not operate the PCIe interface at the 5.0 GT/s Data Rate.
Option 3:
Use an external clock source to supply the PCIe Reference Clock to both the Root Complex and End Point Devices of the Link.
Internal Note:
When measuring the Refclk output, the SerDes should be configured in the A2 state to power-down the TX/RX. This is consistent with the test methodology applied to external Refclk generators.