SPRZ255F May   2007  – June 2020 TMS320F28044

 

  1.   TMS320F28044 Digital Signal Processor Silicon Revision 0
    1. 1 Introduction
    2. 2 Device and Development Tool Support Nomenclature
    3. 3 Device Markings
    4. 4 Silicon Change Overview
    5. 5 Usage Notes and Known Design Exceptions to Functional Specifications
      1. 5.1 Usage Notes
        1. 5.1.1 PIE: Spurious Nested Interrupt After Back-to-Back PIEACK Write and Manual CPU Interrupt Mask Clear
      2. 5.2 Known Design Exceptions to Functional Specifications
    6. 6 Documentation Support
  2.   Trademarks
  3.   Revision History

Device and Development Tool Support Nomenclature

To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of all TMS320™ DSP devices and support tools. Each TMS320 DSP commercial family member has one of three prefixes: TMX, TMP, or TMS (for example, TMS320F28044). Texas Instruments recommends two of three possible prefix designators for its support tools: TMDX and TMDS. These prefixes represent evolutionary stages of product development from engineering prototypes (TMX/TMDX) through fully qualified production devices/tools (TMS/TMDS).

TMX Experimental device that is not necessarily representative of the final device's electrical specifications
TMP Final silicon die that conforms to the device's electrical specifications but has not completed quality and reliability verification
TMS Fully qualified production device

Support tool development evolutionary flow:

TMDX Development-support product that has not yet completed Texas Instruments internal qualification testing
TMDS Fully qualified development-support product

TMX and TMP devices and TMDX development-support tools are shipped against the following disclaimer:
"Developmental product is intended for internal evaluation purposes."

TMS devices and TMDS development-support tools have been characterized fully, and the quality and reliability of the device have been demonstrated fully. TI's standard warranty applies.

Predictions show that prototype devices (TMX or TMP) have a greater failure rate than the standard production devices. Texas Instruments recommends that these devices not be used in any production system because their expected end-use failure rate still is undefined. Only qualified production devices are to be used.

TI device nomenclature also includes a suffix with the device family name. This suffix indicates the package type (for example, GGM) and temperature range (for example, A).