• Menu
  • Product
  • Email
  • PDF
  • Order now
  • AM62Lx Escape Routing for PCB Design

    • SPRADI2 March   2025 AM62L

       

  • CONTENTS
  • SEARCH
  • AM62Lx Escape Routing for PCB Design
  1.   1
  2.   Trademarks
  3. 1 Introduction
  4. 2 Via Channel Arrays
  5. 3 Width/Spacing Proposal for Escapes
  6. 4 Stackup
  7. 5 Via Sharing
  8. 6 Floorplan Component Placement
  9. 7 Critical Interfaces Impact Placement
  10. 8 Routing Priority
  11. 9 SerDes Interfaces
  12. 10DDR Interfaces
  13. 11Power Decoupling
  14. 12Route Lowest Priority Interfaces Last
  15. 13Summary
  16. 14Revision History
  17. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Application Note

AM62Lx Escape Routing for PCB Design

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

AM62Lx is an extension of the low-power, low-cost Sitara Industrial/Auto grade family of processors. AM62Lx is based on the Cortex-A53 microprocessor, alongwith extensive peripheral and networking options for a variety of embedded applications. AM62Lx is available in a 11.9mm x 11.9mm VCA package with a mix of 0.5mm ball pitch. The package BGA design is built leveraging TI Via Channel Array Technology (VCA) technology, which enables package miniaturization while still utilizing low cost PCB routing rules. Via Channel Array (VCA) is built with careful considerations on escape routing to avoid costly High-Density Interconnect (HDI) and expensive Via technologies. This document is intended to provide a reference for escape routing on the AM62Lx device. Care must be taken to route signals with special requirements such as DDR, high speed interfaces. Refer to the High-Speed Interface Layout Guidelines and DDR Routing Guidelines for more details. Details on Power Delivery Network are provided in AM62Lx PDN Application note and any routing and layout requirements specified in those documents supersede the generic requirements provided here.

2 Via Channel Arrays

Via Channel Array Technology has been successfully used in a variety of TI products that minimizes package dimensions by using smaller ball pitch and utilizing low cost PCB routing. Via Channel technology enables routing channels to escape innermost BGA positions. This has several advantages. First, the via outside diameter (also known as the annular ring) can be larger than it normally would be if it had to be placed between the BGAs in a tighter pitch, because all the vias are placed in special areas called via channels. This makes PCB manufacturing less expensive, because larger vias are possible. Second, the vias are grouped in a radial pattern instead of a series of concentric rings around the middle of the chip, which is the case with normal BGA array PCB routing. The traces are more easily routed out of the inner parts of the chip because they are not restricted to the narrow paths between many rows of vias. The unique outer row routing and the via channel inner routing are two important parts of this technology on the AM62Lx. The AM62Lx BGA Via Channel Array is shown in Figure 2-1.

 AM62Lx BGA Array with Via Channels Figure 2-1 AM62Lx BGA Array with Via Channels

The first row (the outside row) supports any size trace desired, because the trace comes from the PCB ball land and goes out on the PCB. Normally, the second row traces must be routed in between the first row of the PCB ball lands. The AM62Lx parts allow a 3.2 mil trace/space on interior layers and 3.7 mil/4 mil trace width/space on exterior layers.

Figure 2-2 shows the first two rows of the AM62Lx package and how it is possible to route 3.2 mil traces and spaces in the areas between balls.

 Outer Rows of Traces Figure 2-2 Outer Rows of Traces

Starting at the third row, as with any BGA package, vias are necessary. As stated earlier, the vias are gathered in the via channels, so the only vias that need to be placed in between balls are some of the power vias in areas of ground or power copper pour. In this case, they have no regular via ring because they are located in an area of copper pour where all the surrounding balls share the same net. This is elaborated more in the later section with details on via sharing. Because the via ring is larger than one that would normally fit in between these balls with the required clearance, the layout tool may flag a design rule check (DRC) error; however, this is a false warning because there is no risk of shorting to a nearby pad as they are all on the same net. The rest of the vias must be placed into the via channels as shown below. Figure 2-3 shows how the vias are grouped in the via channels.

 Vias in Via Channels Figure 2-3 Vias in Via Channels

3 Width/Spacing Proposal for Escapes

The AM62Lx via channel array solution has been designed to support the following. The AM62Lx package supports a similar feature set as several other competition solutions with approximately 15% smaller package area and ~10% wider line width. This solution thus reduces PCB foot print and uses lower cost PCB rules, enabling compact and low-cost systems.

Table 3-1 Width/Spacing Proposal for Escapes
PCB Feature PCB Routing Requirements
Minimum via pad diameter 18 mils
Via hole size 8 mils
Minimum trace width/spacing required in the BGA break out

External Layers: 3.2 mil/3.2 mil

Internal Layers: 3.7 mil/4 mil

Number of layers used for escape 4
BGA land pad size 10 mils
Package Size 11.9mm x 11.9mm, 0.5mm pitch w/ VCA
PCB layers (signal routing, total) recommended 2, 6 (Excluding signal escapes on top layer)
Solder resist clearance 12 mils (1 mil annular)

4 Stackup

PCB stack-up is one of the first and most important considerations in realizing a successful PCB. AM62Lx device supports a BGA array or 23x23 with a 0.5mm pitch and a body size of 11.9mm. PDN compliance and robustness is critical to meet all the performance objectives of the device and associated peripherals. To enable this, TI recommends allocating one layer for power planes. Ground planes must be added adjacent to the power planes and adjacent to the outer layers for shielding and controlled impedance routing. High speed interfaces such as DDR, DSI, and USB require ground planes for impedance matching. Additionally, to meet the DDR interface speeds, ground layers to reference the DDR signals are strongly recommended. The escapes on the AM62Lx board design were achieved with 6 layers, as shown below.

Table 4-1 Example PCB Layer Stack-up
PCB Layer Layer Routing, Planes or Pours
TOP Component pads, Ground and signal escapes
Layer 2 Ground
Layer 3 Signal Routing
Layer 4 Power Routing
Layer 5 Power/Ground reference
BOTTOM Ground, Power, Signal and component pad routing

The AM62Lx board design example provided is implemented in a 6-layer stack-up as described above. This board is designed for optimum signal integrity on the high-speed interfaces while limiting the board size. The AM62Lx board is implemented without HDI (High Density Interconnect) and does not use micro vias, which are both intended to save board cost. All vias on the AM62Lx board are Plated Through Hole (PTH) and pass completely through the board. Additionally, via-in-pad design rules which add cost to the board are avoided. Proper analysis shall be performed to validate both signal and power integrity, if further optimizations are required to reduce PCB stack-up and/or routing rules illustrated in this document.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale