SNVU762 May   2021

 

  1.   1
  2.   2
  3.   3
    1.     4
    2.     5
  4.   6
    1.     7
    2.     8
    3.     9
    4.     10
    5.     11
  5.   12
    1.     13
    2.     14
    3.     15

Graphical User Interface (GUI) Guidance

The LP586x GUI is a convenient tool to control and evaluate all functions of LP586x family. Open the LP586x.exe file and plug the USB cable into the USB port of the computer. The GUI automatically connects with the LP5860EVM. Figure 3-1 illustrate the status bar showing the connection status at the bottom of GUI. Hardware Connected shows in the status and the indicator in the USB2ANY stops blinking when successfully connected. Click the connection button to connect or disconnect the LP5860EVM with the GUI.

GUID-20210507-CA0I-3NF4-LW04-1JXNXM536VBH-low.svg Figure 3-1 Status Bar

If the USB2ANY has not been previously used to evaluate the LP5860EVM, a correlating firmware (FW) version must be updated into USB2ANY. Following the instructions in the GUI when plugging in the USB cable can update the FW successfully, see Figure 3-2.

GUID-20210507-CA0I-JRPG-56PC-CMPVPSQFTJHK-low.svg Figure 3-2 Firmware Update