SNOAA76 August   2021 LDC3114 , LDC3114-Q1

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Benefits of Inductive Proximity Sensing
    2. 1.2 Common Applications
    3. 1.3 Human-Machine Interface Design Guide
  3. 2System Considerations
    1. 2.1 Target Properties
    2. 2.2 Sensing Distance
    3. 2.3 LDC3114 Device Features
  4. 3Design
    1. 3.1 Sensor Size and Frequency
    2. 3.2 Linear Sensing Region
  5. 4Measured Raw Data Output
    1. 4.1 Measured Response of LDCCOILEVM Sensor N
    2. 4.2 Measured Response of LDCCOILEVM Sensor R
  6. 5Observed Effects of Ambient Temperature
  7. 6References

Target Properties

To achieve the best sensing response, the metal target should be at least the size of the sensing coil. It is also important to choose a highly conductive metal, such as copper or aluminum, because these have stronger inductive responses.

Figure 2-1 shows the sensor frequency shift of several common metals as a function of distance. Any discontinuities in the metal (gaps, voids, or indents) should be avoided, as they can cause disruptions in the current path and lead to measurement noise.

GUID-8CCD4A99-2D7A-4446-A103-75042EFEBF29-low.gif Figure 2-1 Sensor Frequency vs Distance of Common Targets

In regards to target thickness, it is a general guideline that it should be at least 3 skin depths. Skin depth, δ, is the distance where the eddy currents are reduced to approximately 37% of the density at the surface.

For further details on target design and calculating skin depth, refer to the LDC Target Design application report.