SNOAA04A March   2020  – June 2021 FDC1004 , FDC1004-Q1 , FDC2112 , FDC2112-Q1 , FDC2114 , FDC2114-Q1 , FDC2212 , FDC2212-Q1 , FDC2214 , FDC2214-Q1 , LDC0851 , LDC1041 , LDC1051 , LDC1101 , LDC1312 , LDC1312-Q1 , LDC1314 , LDC1314-Q1 , LDC1612 , LDC1612-Q1 , LDC1614 , LDC1614-Q1 , LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1

 

  1.   Trademarks
  2. 1Introduction
  3. 2Inductive Sensor Simulation
  4. 3Using the Electromagnetic Problem Answer File
  5. 4Calculating Resolution
  6. 5Other Resources
  7. 6Summary
  8. 7References
  9. 8Revision History

Other Resources

For inductive sensing simulations, the Excel_FEMM tool can be especially helpful to speed up the simulation process.

For basic target shapes, the tool can automate the simulation process and will output the simulation results. It can also be useful to automate the creation of the coil in FEMM, and the resulting .fem file can be modified for custom target shapes. This tool is included with the LDC Tools Excel calculator.

For more general instructions and help using FEMM, please see the Finite Element Method Magnetics : Homepage.