SNIK005 august   2023 TMP9R00-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2SEE Mechanisms
    1. 2.1 Test Device and Test Board Information
  6. 3Irradiation Facility and Setup
    1. 3.1 SEL Results
    2. 3.2 SET Results
      1. 3.2.1 Histogram of Temperature Events Exceeding ±1.5°C
    3. 3.3 Event Rate Calculations
  7. 4Summary

SEL Results

During SEL characterization, the device was heated using forced hot air, maintaining the die temperature at 125°C. The temperature was monitored by means of a K-type thermocouple attached as close as possible to the die. The species used for the SEL testing was a Thulium ion with angle of incidence at 0° and 29° for an LETEFF = 66 and 75 MeV-cm2/mg. A flux of approximately 105 ions/cm2 -s and a fluence of approximately 107 ions were used for all runs. The VCC voltage was set to the recommended maximum at 2.0 V. No SEL events were observed during both runs, as shown in Table 3-2. The resulting graph of current vs time is detailed in Figure 3-1.

Table 3-2 TMP9R00-SP SEL Conditions Using Tr with Angle = 0° and 29°
Run # Distance (mm) Temperature
(°C)
Ion Type Angle of Incidence Flux
(ions·cm2/mg)
Fluence
(ions/cm2)
LETEFF
(MeV-cm2/mg)
1 40 125 Tr 0° 1.00 × 105 1.00 × 107 66
2 40 125 Tr 29° 1.00 × 105 1.00 × 107 75
GUID-20FAA77A-8FE9-4653-9C95-9855782E87CB-low.png Figure 3-1 Current vs Time for VCC Supply During SEL Run #2