SNAU282 September 2022
The Other page contains some registers to control the GPIO pins of the LMK04832. Each pin has two fields, the first is the _TYPE field which allows the input or output mode of the pin to be defined. The second is the _MUX field which, when set for output, controls what the pin will output.
Figure 11-10 TICS Pro
- Other Page