SLYU065
March 2023
Abstract
Trademarks
1
Overview
1.1
Kit Contents
1.2
Related Documentation From Texas Instruments
2
Hardware
2.1
Features
3
Operation
3.1
Quick Start Setup
3.2
EVM Operation
3.2.1
Software Setup
3.2.1.1
Driver Installation
3.2.1.2
Firmware
3.2.1.2.1
Firmware Debug
3.2.1.3
GUI Setup and Usage
3.2.1.3.1
Initial Setup
3.2.1.3.2
GUI Operation
4
Schematics, PCB Layout, and Bill of Materials
4.1
Schematics
4.2
PCB Layout
4.3
Bill of Materials
3.1
Quick Start Setup
Download and install the PAMB
Windows®
USB driver:
http://www.ti.com/lit/zip/sbac253
.
Attach the EVM to the Sensor Control Board (TI-SCB) (see
Figure 3-1
).
TI-SCB
must be ordered separately.
Apply a magnetic field to the sensor by doing one of the following:
Connect the Rotate & Push module by attaching to the EVM (see
Figure 3-10
).
Mount the EVM with the sensors aligned to the axis of rotation of a rotating magnet.
Connect the EVM to a PC using a USB cable.
Insert the micro USB cable into the TI-SCB Controller onboard USB receptacle J2.
Plug the other end of the USB cable into a PC.
Access the GUI from the following link in either a
Firefox™
or
Google Chrome™
browser:
TMAG6180-6181EVM GUI:
https://dev.ti.com/gallery/search/TMAG6180-6181
.
Select a device to test
Click plots icon to advance to main device interface.
EVM GUI defaultS to TMAG6180.
Click
Collect Data
Observe the outputs in the GUI. See
Section 3.2.1.3
for more information on GUI setup and operation.