SLVUDM3 February   2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Setup
    3. 2.3 Interfaces
  9. 3Software
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks

Power Requirements

Follow these steps to set up the power supply:

  1. Connect 5.5V power supply to the power jack (PWR_JACK) connector (J18) of the TRF-X-AFE7950EVM.
  2. Check that the D9 (PWR) LED light is on. The power supply draws approximately 1600mA.
  3. Connect a USB type mini-B cable from the PC to the USB port (J19) of the TRF-X-AFE7950EVM.
  4. Check that the D10 (USB_PWR) LED light is on. The LED light strength depends on the USB cable length. If the LED light is not on, then use a shorter USB cable. TI tested the EVM with a three-foot USB cable.
  5. The power-supply sequencer on the TRF-X-AFE7950EVM has a power status for each rail. If the power good (PGOOD) is logic high, then the corresponding power supply rail is powered correctly. The respective LED lights are on. Check that the following LEDs lights are on.
    • D5 (1P8) LED
    • D6 (1P2) LED
    • D7 (0P9) LED
    • D8 (3P3_LMK) LED