SLVUBU6A April 2020 – June 2020
An external resistor is used to convert a proportional load current into a voltage, which is compared with an internal reference voltage. When the voltage on the CL pin exceeds the reference voltage, the current is clamped.
The inherent current limit (Ilim,nom) is still present when using an external current limit. The smaller one of the internal or external set value decides the actual nominal current limit. If it is decided to not use an external programmable current, tie the CL pin to ground.
Equation 2 is the equation of the current limit resistor.
R32 is a 2kΩ resistor; R33 is a 1kΩ resistor, and R8 is a 0Ω resistor. Populate/depopulateR8, R32, and R33 to vary CL. When 0Ω, there is no external current limit function, the internal current limit is active.