SLVU703A August 2012 – September 2021
The board layout for the TPS54395EVM is shown in Figure 5-1 through Figure 5-6. The top layer contains the main power traces for VIN and VOUTx. Also on the top layer are connections for the pins of the TPS54395 and a large area filled with ground. Many of the signal traces also are located on the top side. The input decoupling capacitors are located as close to the IC as possible. The input and output connectors, test points, and all of the assembled components are located on the top side. An analog ground (GND) area is provided on the top side. Analog ground (GND) and power ground (PGND) are connected at a single point on the top layer near the IC. The other layers are primarily power ground but the bottom layer has some traces to connect the test points for SSx and ENx.
Figure 5-1 Top Assembly
Figure 5-2 Top Layer
Figure 5-3 Internal 1 Layer
Figure 5-4 Internal 2 Layer
Figure 5-5 Bottom Layer
Figure 5-6 Bottom Assembly