SLVU380A September 2010 – October 2021
The board layout for the TPS54320 is shown in Figure 3-1 through Figure 3-3. The topside layer of the EVM is laid out in a manner typical of a user application. The top and bottom layers are 2-oz. copper.
The top layer contains the main power traces for PVIN, VIN, VOUT, and VPHASE. Also on the top layer are connections for the remaining pins of the TPS54320 and a large area filled with ground. The bottom ground layer contains a ground plane only. The top side ground traces are connected to the bottom ground plane with multiple vias placed around the board including nine vias directly under the TPS54320 device to provide a thermal path from the top-side ground plane to the bottom-side ground plane.
The input decoupling capacitors (C2, and C3) and bootstrap capacitor (C5) are all located as close to the IC as possible. In addition, the voltage set-point resistor divider components are also kept close to the IC. The voltage divider network ties to the output voltage at the point of regulation, the copper VOUT trace at the J3 output connector. For the TPS54320, an additional input bulk capacitor may be required, depending on the EVM connection to the input supply. Critical analog circuits such as the voltage setpoint divider, frequency set resistor, slow start capacitor and compensation components are terminated to ground using a wide ground trace separate from the power ground pour.
Figure 3-1 TPS54320 Top-Side Layout
Figure 3-2 TPS54320 Bottom-Side Layout
Figure 3-3 TPS54320 Top-Side Assembly