SLVSCP6H July 2014 – June 2020
PRODUCTION DATA.
To prevent sudden changes in the torque applied to the motor which could result in acoustic noise, the DRV10983 provides the option of limiting the maximum rate at which the speed command changes. ClsLpAccel[2:0] can be programmed to set the maximum rate at which the speed command changes (shown in Figure 26).
Figure 26. Closed-Loop Accelerate