SLVK172 June   2024 TPS7H3014-SP

 

  1.   1
  2.   TPS7H3014-SP Single-Event Effects (SEE)
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Depth, Range, and LETEFF Calculation
  9. 6 Test Setup and Procedures
  10. 7 Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-Up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 8 Single-Event Transients (SET)
  12. 9 Event Rate Calculations
  13. 10Summary
  14.   A References

Single-Event Latch-Up (SEL) Results

During SEL characterization, the device was heated using a closed-loop PID controlled heat gun [MISTRAL 6 System (120V, 2400W)]. The DUT temperature was monitored prior to being irradiated with a FLIR IR-camera to ensure the junction temperature. The species used for SEL testing was 165Ho. Incident angle was used which achieved an LETEFF of 75MeV·cm2/mg.

Three devices were tested under the loopback mode (for more details in loopback mode refer to footnote 1). In the loopback mode (used for DSEE) the overdrive voltage was selected to be 1V. This was done to avoid interpreting a transient as a functional interrupt. All devices were tested in the Waiting to Sequence DOWN state. Maximum recommend voltages were used for VIN, VPULL_UPx and VUP. For more configuration information please refer to Table 6-1.

Not a single functional interrupt was observed, neither a high current event on either of the power supplies of the TPS7H3014-SP. A total of three units were tested under the same conditions and configuration. This indicates the TPS7H3014-SP is SEL-free. The results for three runs across three devices are shown in Table 8-3. A typical VIN current vs time plot during a SEL run is shown in Figure 7-1. Typical VPULL_UPx current vs time plots during SEL runs are shown in Figure 7-2 and Figure 7-3.

Table 7-1 Summary of TPS7H3014-SP SEL Test Condition and Results
RUN # UNIT # ION LETEFF (MeV·cm2/mg)

FLUX

(ions·cm2/mg)

FLUENCE

(NUMBER OF IONS)

SEL

(NUMBER OF EVENTS)
1 1

165Ho

75

2.57 × 104

1.00 × 107

0

2 2

165Ho

75

1.62 × 104

1.00 × 107

0

3 3

165Ho

75

8.70 × 104

1.00 × 107

0

Using the MFTF method described in Single-Event Effects (SEE) Confidence Interval Calculations application report and combining (or summing) the fluence of the four runs @ 125°C (4 × 107), the upper-bound cross-section (using a 95% confidence level) is calculated as:

σSEL ≤ 1.23 × 10–7cm2/device for LETEFF = 75MeV·cm2/mg and T = 125°C.

TPS7H3014-SP Current vs Time for
                        IIn: Run #1 of the TPS7H3014-SP at T = 125°C Figure 7-1 Current vs Time for IIn: Run #1 of the TPS7H3014-SP at T = 125°C
TPS7H3014-SP Current vs Time for
                        VPULL_UP1: Run #1 of the TPS7H3014-SP at T = 125°C Figure 7-2 Current vs Time for VPULL_UP1: Run #1 of the TPS7H3014-SP at T = 125°C
TPS7H3014-SP Current vs Time for VPULL_UP2: Run #1 of the
                    TPS7H3014-SP at T = 125°C Figure 7-3 Current vs Time for VPULL_UP2: Run #1 of the TPS7H3014-SP at T = 125°C