SLVK099B March   2022  – September 2023 TPS7H5001-SP , TPS7H5002-SP , TPS7H5003-SP , TPS7H5004-SP

PRODUCTION DATA  

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Depth, Range, and LETEFF Calculation
  9. 6 Test Setup and Procedures
  10. 7 Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-Up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 8 Single-Event Transients (SET)
    1. 8.1 System Level Implications
  12. 9 Event Rate Calculations
  13. 10Summary
  14.   A Total Ionizing Dose from SEE Experiments
  15.   B References
  16.   C Revision History

Single-Event Transients (SET)

SET are defined as heavy-ion-induced transients upsets on the OUTX, SRX, SS, and Error Amp (while in unity gain) of the TPS7H500x-SP.

Testing was performed at room temperature (no external temperature control applied). The heavy-ions species used for the SET testing were Krypton (84Kr), Silver (109Ag), Praseodymium (141Pr), and Holmium (165 Ho) for an LETEFF = 30 to 75 MeV·cm2/mg. For more details, see Ion LETEFF, Depth, and Range in Silicon. Flux of 7.75 × 104 to 1.65 × 105 ions/cm2·s and a fluence of 9.97 × 106 to 1 × 107 ions/cm2, per run were used for the SET characterization.

SET testing was categorized as:

  1. VIN = 12 V (nominal) at FSW = 500 kHz

    (All TPS7H500X-SP devices)

    .
  2. VIN = 14 V (max) at FSW = 500 kHz.
  3. VIN = 4 V at FSW = 500 kHz.
  4. Error amplifier.
  5. Cross conduction at FSW = 500 kHz.
  6. VIN = 4 V (min) at FSW = 500 kHz using an external clock with RT = open.
  7. VIN = 14 V (max) at FSW = 500 kHz using an external clock with RT = open.
  8. VIN = 4 V (min) 12 V (nominal) and 14 V (max) at FSW = 1 MHz using the internal clock with RT = 90.9 kΩ.
  9. VIN = 4 V (min) 12 V (nominal) and 14 V (max) at F SW= 2 MHz using the internal clock with RT = 38.3 kΩ.

As the list shows, the only SET case that was repeated for the TPS7H5002/3/4-SP devices was the 12-V nominal at FSW = 500 kHz case. All other SET cases were conducted with the TPS7H5001-SP. This was done due to how closely the TPS7H5002/3/4 devices correlated SET wise to the original TPS7H5001-SP device, specifically having similar number of OUTA and SRB transients and the same found onset.

Cross conduction is a concern in synchronous converter applications due to the possibility of a short circuit during an SET upset. In addition to the hardware X-conduction testing, all recorded upsets during all runs discussed on this report (SEL, SEB, and SET) were verified for such conditions when possible. Using software, cross conduction was verified for:

  1. OUTA to SRA.
  2. OUTB to SRB.
  3. OUTA to OUTB.

The PWM signals were converted to digital levels by comparing the voltage levels of the recorded upset to an VIH = 1.89 V (VIH from the LMG1205 GaN driver was used). If the signals were greater than this voltage, a digital one was returned. Otherwise, a logical 0 was recorded. After the signals were converted into a digital value array, a BITAND was implemented using the desired waveforms. If any logical 1 was present on the resulting response, a cross conduction was said to occur. Not a single upset of this kind was recorded across all upsets and all runs including SEL, SEB, and SET.

Table 8-1 shows waveform size, sample rate, trigger type, value, and signal for all scopes used. For SS, not a single capture was recorded under the conditions used for the data collection. For this reason, the data is not presented in the table.

Table 8-1 Scope Settings Note: Only one signal was used as a trigger source at a time, this table just present all possible sources for a given scope, the same is valid for the trigger type. All percentage specified on the trigger value are deviation from the nominal value.
Scope Model Trigger Signal Trigger Type Trigger Value Record Length Sample Rate
DPO7104C OUTA Pulse-Width (Outside) ±30% 500 ns/div or 2 μs/div 2.5 or 5 GS/s
COMP Window (Outside) ±10%
AND Gate (X-Conduction) Edge-Positive 2.5 V
PXIe-5110 SRB Pulse-Width (Outside) ±30% 4 kS 100 MS/s
PXIe-5162 SS Edge/Negative 0.6 100 kS 2.5 MS/s

VIN = 12 V (Nominal) at FSW = 500 kHz

For VIN = 12 V and switching frequency of 500 kHz, the results are presented in Table 8-4. The outside-pulse width trigger was set to 30% from the nominal pulse width for both the DPO7104C and the PXIe-5110. Upper-bound cross section at 95% confidence interval and based on SLVK047 are presented in Table 8-3 and Table 8-4. The cross-section plot for this case and Weibull parameter are shown in Figure 8-1 and Table 8-5, respectively. A typical time domain plot for OUTA is shown in Figure 8-2. Since the main concern for a DC-DC converter is the OUTX, (OUTA and OUTB have similar if not equal performance), the OUTA signal was used to characterize the Onset. Due to SRX performing worse behavior than OUTX, the onset was not found during testing. To accurately determine the onset for SRX, a Weibull fit plot was created. Conditions and the Weibull fit plot for SRB are shown below with the remaining 12-V 500-kHz results.

Table 8-2 Summary of TPS7H500x-SP SET Test Condition and Results VIN = 12 V There is a greater focus on OUTX transients than on SRX transients because OUTX transients have more implication at a system level. This is discussed more in the "System Level Implications" section, please refer to this section for more details.

For the TPS7H5002/3-SP SRA instead of SRB was monitored.

Run NumberDeviceUnit NumberIon

LETEFF (MeV·cm2/mg)

Flux (ions·cm2/mg)Fluence (Number of Ions)Number of DPO7104C ≥ 30% (OUTANumber of PXIe-5110 ≥ 30% (SRB)
11TPS7H50013165Ho751.20 × 1051 × 107114N/A
12TPS7H50014141Pr751.07 × 1051 × 10796464
13TPS7H50014141Pr651.06 × 1059.99 × 10691409
14TPS7H50012141Pr759.51 × 1041 × 107108532
15TPS7H50012141Pr651.03 × 1051 × 10779414
16TPS7H50013109Ag481.22 × 1059.98 × 10630N/A
17TPS7H50013109Ag481.39 × 1059.96 × 1069N/A
18TPS7H50013109Ag481.29 × 1059.98 × 106N/A300
19TPS7H50014109Ag488.27 × 1041 × 10712286
20TPS7H5001784Kr401.36 × 1059.95 × 1063273
21TPS7H5001784Kr371.24 × 1059.99 × 1060249
22TPS7H5001784Kr301.37 × 1059.96 × 1060245
82TPS7H50029165Ho741.13 × 1051 × 10784577
83TPS7H500310165Ho751.19 × 1051 × 10796546
84TPS7H500411165Ho751.14 × 1059.99 × 106104N/A
85TPS7H5002984Kr301.12 × 1059.96 × 1060212
86TPS7H50031084Kr301.06 × 1059.95 × 1060216
87TPS7H50041184Kr301.05 × 1051 × 1070N/A
Table 8-3 Upper Bound Cross Section for OUTA for VIN= 12 V and FSW = 500 kHz Based on TPS7H5001-SP Upper Bound Cross Section was at 95% confidence interval and based on SLVK047.
LETEFF (MeV·cm2/mg)Number of UpsetsUpper Bound X-Section (cm2)
3003.70 × 10-7
3703.69 × 10-7
4038.81 × 10-7
48512.24 × 10-6
651709.88 × 10-6
753181.18 × 10-5
Table 8-4 Upper Bound Cross Section for SRB for VIN= 12 V and FSW = 500 kHz Based on TPS7H5001-SP Upper Bound Cross Section was calculated at 95% confidence interval and based on SLVK047.
LETEFF (MeV·cm2/mg)Number of UpsetsUpper Bound X-Section (cm2)
302452.79 × 10-5
372492.82 × 10-5
402733.09 × 10-5
485863.18 × 10-5
658234.41 × 10-5
759965.30 × 10-5
GUID-20220119-SS0I-NWZM-F86L-5Z4HLJSVCHTW-low.jpg

Upper and lower bound were calculated to 95% confidence. Weibull fit was done for the mean value.

Figure 8-1 Cross Section and Weibull Fit for SRB at VIN = 12 V and FSW= 500 kHz
Table 8-5 Weibull Parameter for SRB at VIN= 12 V and FSW= 500 KHz
ParameterValue
Upper Bound X-Section5.30 × 10-5
X-Sat4.98 × 10-5
Onset14
W20
s1.5
GUID-20220119-SS0I-FHNL-JFKX-KTH2SSMJ7THR-low.png Figure 8-2 Worst Case OUTA Time Domain Upset (Run Number 14)
GUID-20220119-SS0I-Z8KL-67TZ-SNMCCNJHJPJ5-low.png Figure 8-3 OUTA Normalized Percentage Pulse Width Deviation During Trigger
GUID-20220119-SS0I-PWL5-ZJJC-BZCNRCXXR9KB-low.png Figure 8-4 OUTA Duration of Triggers (µs)
GUID-20220119-SS0I-SF2D-WVB6-PXL1DSXQM68G-low.png Figure 8-5 Worst Case SRB Time Domain Upset (Run Number 14)
GUID-20220119-SS0I-ZV3S-PP10-VV5JRVTHNLRJ-low.png Figure 8-6 SRB Normalized Percentage Pulse Width Deviation During Trigger
GUID-20220119-SS0I-CDTR-T6XM-NHLDCJPRJSHJ-low.png Figure 8-7 SRB Duration of Triggers (µs)

VIN= 14 V (Maximum) at FSW= 500 kHz

Table 8-6 Summary of TPS7H5001-SP SET Test Condition and Results VIN = 14 V
Run NumberUnit NumberIonLETEFF (MeV·cm2/mg)FLUX (ions·cm2/mg)Fluence (Number of Ions)Number DPO7104C ≥ 30% (OUTA)Number PXIe-5110 ≥ 30% (SRB)
234141Pr758.85 × 1049.97 × 106100496
244141Pr751.03 × 1059.99 × 10693494
254141Pr651.11 × 1059.97 × 10661400
262141Pr751.09 × 1051.00 × 107120488
272141Pr651.04 × 1051.00 × 10780372
284109Ag488.19 × 1041.00 × 10713290
29784Kr371.17× 1051.00 × 1071232

VIN=4-V (Min) at FSW = 500 kHz

Table 8-7 Summary of TPS7H5001-SP SET Test Condition and Results VIN = 4-V
Run Number Unit Number Ion LETEFF
(MeV·cm2/mg)
Flux
(ions·cm2/mg)
Fluence
(Number of Ions)
Number of DPO7104C ≥ 30% (OUTA) Number of PXIe-5110 ≥ 30% (SRB)
30 4 141Pr 75 1.09 × 105 1.00 × 107 111 617
31 4 141Pr 65 1.19 × 105 1.00 × 107 25 424
32 4 141Pr 65 1.09 × 105 1.00 × 107 112 479
33 4 141Pr 65 1.15 × 105 9.98 × 106 76 451
34 2 141Pr 75 7.66 × 104 1.00 × 107 109 577
35 2 141Pr 65 1.00 × 105 1.00 × 107 79 474
36 4 109Ag 48 9.38 × 104 1.00 × 107 22 306
37 7 84Kr 37 1.35 × 105 9.98 × 106 0 210

Error Amp in Unity Gain

Time Domain Plots for the COMP voltage and Normalized max Value for each upset is shown on Nominal Trigger on COMP Run Number 43 VIN = 12 V

Table 8-8 Summary of TPS7H5001-SP SET Test Condition and Results for the Error Amplifier in Unity Gain.
Run NumberUnit NumberVIN (V)IonLETEFF (MeV·cm2/mg)Flux (ions·cm2/mg)Fluence (Number of Ions) Number of Upsets COMP ≥ |10|%
38814141Pr751.53 × 1051.00 × 10711
39812141Pr751.65 × 1051.00 × 1070
4084141Pr751.51 × 1051.00 × 1070
4184141Pr651.30 × 1051.00 × 1070
42812141Pr651.41 × 1051.00 × 1070
43814141Pr651.32 × 1051.00 × 10732
GUID-20220119-SS0I-ZNF7-2K1V-JS337MW3L8TJ-low.png Figure 8-8 Nominal Trigger on COMP Run Number 43 VIN = 12 V
GUID-20220119-SS0I-G9JP-9CQT-GRXWKR8Z20G3-low.png Figure 8-9 Comp Peak Percentage Deviation from Nominal of Triggers

Cross-Conduction (Using Hardware) at FSW = 500 kHz

For cross conduction using hardware an AND Gate (model: SN74AHCT1G08DCKR) was used. IN1 was set as OUTA and IN2 was used as SRA. The output of the AND gate was connected to the CH number 1 of the DPO7104C with an edge trigger at 2.5 V. Not a single trigger was capture indicating that the TPS7H500x-SP is cross-conduction free at the conditions tested and presented here. As mention in the SET introduction, all recorded upset were also verified for the cross conduction in software and not a single cross conduction upset was recorded.

Table 8-9 Summary of TPS7H5001-SP SET Test Condition and Results Cross-Conduction
Run NumberUnit NumberVIN (V)IonLETEFF (MeV·cm2/mg)Flux (ions·cm2/mg)Fluence (Number of Ions)DPO7104C Number Of Upsets
4434141Pr751.20 × 1059.97 × 1060
45312141Pr751.24 × 1059.98 × 1060
46314141Pr751.23 × 1051.00 × 1070

FSW = 500 kHz using an External Clock with RT = Open

Table 8-10 Summary of TPS7H5001-SP SET Test Condition and Results With External Clock
Run NumberUnit NumberVIN (V)IonLETEFF (MeV·cm2/mg)Flux (ions·cm2/mg)Fluence (Number of Ions)Number DPO7104C ≥ 30% (OUTA)Number PXIe-5110 ≥ 30% (SRB)
4724141Pr751.17 × 1051.00 × 1072351
48212141Pr751.25 × 1051.00 × 1072228
49214141Pr751.19 × 1051.00 × 10718
5024141Pr651.07 × 1051.00 × 10711
51212141Pr651.21 × 1051.00 × 10712
52214141Pr651.18 × 1051.00 × 10713
5324109Ag481.00 × 105

9.98 × 106

00
54212109Ag488.96 × 1041.00 × 10700
55214109Ag489.30 × 1041.00 × 10700
GUID-20220119-SS0I-1RQS-0WHP-JSTBW1FLP12B-low.png Figure 8-10 Worst Case OUTA Time Domain Upset (Run Number 48)
GUID-20220119-SS0I-BFN3-M00P-GTFSD8TDJTPP-low.png Figure 8-11 OUTA Normalized Percentage Pulse Width Deviation During Trigger With External Clock
GUID-20220119-SS0I-8QN3-60SM-CDK9G6QBLL9G-low.png Figure 8-12 OUTA Duration of Triggers (µs) With External Clock
GUID-20220119-SS0I-MCZL-QSDD-6QH3PPMQQ9SN-low.png Figure 8-13 Worst Case SRB Time Domain Upset (Run Number 48)
GUID-20220119-SS0I-CFMW-DRR5-0B6QTBPXQGMX-low.png Figure 8-14 SRB Normalized Percentage Pulse Width Deviation During Trigger With External Clock
GUID-20220119-SS0I-JJG7-317Q-F9BZGMN9BS2K-low.png Figure 8-15 SRB Duration of Triggers (µs) With External Clock

FSW = 1 MHz Using an Internal Clock with RT = 90.9 kΩ

Table 8-11 Summary of TPS7H5001-SP SET Test Condition and Results Frequency = 1 MHz
Run Number Unit Number VIN (V) Ion LETEFF (MeV·cm2/mg) Flux (ions·cm2/mg) Fluence (Number of Ions) Number DPO7104C ≥ 30% (OUTA) Number PXI 5110 ≥ 30% (SRB)
56 5 4 141Pr 75 8.52 × 104 1.00 × 107 101 443
57 5 12 141Pr 75 8.29 × 104 9.99 × 106 78 422
58 5 14 141Pr 75 8.85 × 104 9.98 × 106 67 402
59 5 4 141Pr 65 8.42 × 104 1.01 × 107 53 381
60 5 12 141Pr 65 8.99 × 104 9.98 × 106 46 328
61 5 14 141Pr 65 1.00 × 105 1.00 × 107 55 342
62 5 4 109Ag 48 9.72 × 104 9.97 × 106 5 273
63 5 12 109Ag 48 9.70 × 104 9.99 × 106 1 260
64 5 14 109Ag 48 8.28 × 104 1.00 × 107 1 247
GUID-20220119-SS0I-J2NB-1PH6-HNHPKQR8LLXX-low.png Figure 8-16 Worst Case OUTA Time Domain Upset (Run Number 57)
GUID-20220119-SS0I-Z55D-FN1B-LWMM7PWPK33P-low.png Figure 8-17 OUTA Normalized Percentage Pulse Width Deviation During Trigger With 1-MHz Internal Clock
GUID-20220119-SS0I-N2J3-PKXC-ZCDJRVRDV8CK-low.png Figure 8-18 OUTA Duration of Triggers (µs) With 1-MHz Internal Clock
GUID-20220119-SS0I-FZ1K-F4MB-3QQLZHPNBQXZ-low.png Figure 8-19 Worst Case SRB Time Domain Upset (Run Number 57)
GUID-20220119-SS0I-LD6V-NQ4Q-FDN1T29PXCKC-low.png Figure 8-20 SRB Normalized Percentage Pulse Width Deviation During Trigger With 1-MHz Internal Clock
GUID-20220119-SS0I-ZD9F-XFMK-1FZPL2PCPZBX-low.png Figure 8-21 SRB Duration of Triggers (µs) With 1MHz Internal Clock

FSW = 2 MHz Using an Internal Clock with RT = 38.3 kΩ

Table 8-12 Summary of TPS7H5001-SP SET Test Condition and Results Frequency = 2 MHz
Run NumberUnit NumberVIN (V)IonLETEFF (MeV·cm2/mg)Flux (ions·cm2/mg)Fluence (Number of Ions)Number of DPO7104C ≥ 30% (OUTA)Number of PXI 5110 ≥ 30% (SRB)
6564141Pr751.05 × 1059.97 × 106144379
66612141Pr759.89 × 1049.99 × 10610299
67614141Pr751.02 × 1059.97 × 10611492
68612141Pr651.06 × 1051.00 × 10724245
69614141Pr651.07 × 1051.00 × 1079260
70612141Pr651.03 × 1051.00 × 10712229
71612109Ag488.82 × 1041.00 × 1079235
72614109Ag488.79 × 1049.98 × 10612534
GUID-20220119-SS0I-PKXM-V6WB-7ZVGPZPJXXZ5-low.png Figure 8-22 Worst Case OUTA Time Domain Upset (Run Number 66)
GUID-20220119-SS0I-WHFK-PVVF-CQTT8TPJQBMQ-low.png Figure 8-23 OUTA Normalized Percentage Pulse Width Deviation During Trigger With 2-MHz Internal Clock
GUID-20220119-SS0I-VR9G-PJKF-SNLSNX6VMVVJ-low.png Figure 8-24 OUTA Duration of Triggers (µs) With 2-MHz Internal Clock
GUID-20220119-SS0I-LZJC-PFS9-D6TSZT7PJXVJ-low.png Figure 8-25 Worst Case SRB Time Domain Upset (Run Number 66)
GUID-20220119-SS0I-0HGD-1RXQ-JHRKG0K1HDZM-low.png Figure 8-26 SRB Normalized Percentage Pulse Width Deviation During Trigger With 2-MHz Internal Clock
GUID-20220119-SS0I-W8XV-BZVJ-MZD3HXNF3B4T-low.png Figure 8-27 SRB Duration of Triggers (µs) With 2-MHz Internal Clock