SLVA745A December   2015  – April 2025 TPS7B4253-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 DDA 8-pin SO PowerPAD Package
    2. 2.2 PWP 20-pin HTSSOP (with exposed thermal pad) Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Modes and Effects Analysis (Pin FMEA)
    1. 4.1 DDA 8-pin SO PowerPAD Package
    2. 4.2 PWP 20-pin HTSSOP (with exposed thermal pad) Package
  7. 5Revision History

PWP 20-pin HTSSOP (with exposed thermal pad) Package

Figure 4-2 shows the TPS7B4253-Q1 pin diagram for the PWP 20-pin HTSSOP (with exposed thermal pad) package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS7B4253-Q1 data sheet.

TPS7B4253-Q1 Pin Diagram (PWP 20-pin HTSSOP (with exposed thermal
                                    pad) Package) Figure 4-2 Pin Diagram (PWP 20-pin HTSSOP (with exposed thermal pad) Package)
Table 4-6 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
OUT 1 Regulation is not possible, the device operates at current limit. The device can cycle in and out of thermal shutdown. B
NC 2 No effect. Normal operation. D
NC 3 No effect. Normal operation. D
NC 4 No effect. Normal operation. D
NC 5 No effect. Normal operation. D
GND 6 No effect. Normal operation. D
NC 7 No effect. Normal operation. D
NC 8 No effect. Normal operation. D
NC 9 No effect. Normal operation. D
FB 10 If FB is directly connected to OUT, regulation is not possible, the device operates at current limit. The device can cycle in and out of thermal shutdown. If FB is connected by a resistor divider, VOUT tracks VIN minus the dropout voltage. B
ADJ 11 Device is disabled, resulting in no output voltage. B
NC 12 No effect. Normal operation. D
NC 13 No effect. Normal operation. D
NC 14 No effect. Normal operation. D
GND 15 No effect. Normal operation. D
NC 16 No effect. Normal operation. D
NC 17 No effect. Normal operation. D
NC 18 No effect. Normal operation. D
EN 19 Device is disabled, resulting in no output voltage. B
IN 20 Power is not supplied to the device. System performance depends on upstream current limiting. B
Table 4-7 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
OUT 1 The device output is disconnected from the load. B
NC 2 No effect. Normal operation. D
NC 3 No effect. Normal operation. D
NC 4 No effect. Normal operation. D
NC 5 No effect. Normal operation. D
GND 6 Ground loop parasitics are increased and transient performance can be degraded. C
NC 7 No effect. Normal operation. D
NC 8 No effect. Normal operation. D
NC 9 No effect. Normal operation. D
FB 10 The error amplifier input is not connected. Output voltage is indeterminate. B
ADJ 11 The device state is unknown. If the device is on, the output voltage is indeterminate. B
NC 12 No effect. Normal operation. D
NC 13 No effect. Normal operation. D
NC 14 No effect. Normal operation. D
GND 15 Ground loop parasitics are increased and transient performance can be degraded. C
NC 16 No effect. Normal operation. D
NC 17 No effect. Normal operation. D
NC 18 No effect. Normal operation. D
EN 19 The enable circuit is in an unknown state. The device can be enabled or disabled. B
IN 20 Power is not supplied to the device. B
Table 4-8 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
OUT 1 NC No effect. Normal operation. D
NC 2 NC No effect. Normal operation. D
NC 3 NC No effect. Normal operation. D
NC 4 NC No effect. Normal operation. D
NC 5 GND No effect. Normal operation. D
GND 6 NC No effect. Normal operation. D
NC 7 NC No effect. Normal operation. D
NC 8 NC No effect. Normal operation. D
NC 9 FB No effect. Normal operation. D
ADJ 11 NC No effect. Normal operation. D
NC 12 NC No effect. Normal operation. D
NC 13 NC No effect. Normal operation. D
NC 14 GND No effect. Normal operation. D
GND 15 NC No effect. Normal operation. D
NC 16 NC No effect. Normal operation. D
NC 17 NC No effect. Normal operation. D
NC 18 EN No effect. Normal operation. D
EN 19 IN Device is always enabled. B
Table 4-9 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
OUT 1 Regulation is not possible. VOUT = VIN. B
NC 2 No effect. Normal operation. D
NC 3 No effect. Normal operation. D
NC 4 No effect. Normal operation. D
NC 5 No effect. Normal operation. D
GND 6 Power is not supplied to the device. System performance depends on upstream current limiting. B
NC 7 No effect. Normal operation. D
NC 8 No effect. Normal operation. D
NC 9 No effect. Normal operation. D
FB 10 Device channel is closed. If FB is tied to OUT, then VOUT = VIN. If FB is connected with a resistor divider, VOUT equals VIN if there is no loading on the device. If the loading on the device exceeds the leakage through the top feedback resistor, VOUT is pulled to 0V. B
ADJ 11 VOUT tracks VIN minus the dropout voltage. B
NC 12 No effect. Normal operation. D
NC 13 No effect. Normal operation. D
NC 14 No effect. Normal operation. D
GND 15 Power is not supplied to the device. System performance depends on upstream current limiting. B
NC 16 No effect. Normal operation. D
NC 17 No effect. Normal operation. D
NC 18 No effect. Normal operation. D
EN 19 Device is always enabled. B
IN 20 No effect. Normal operation. D