SLUUDH3 December 2025 AM62L
Once the connection is established, the user can start collecting power data by navigating to the 'Data' tab. Use 'One-Time' for an instantaneous capture of the power data and use 'Stream' for a continuous readings that update every one second. Click 'Stream' again to stop the capture and review the .csv file generated with the data collected.
Figure 1-2 How to Start Data CaptureTo visualize the data in a graph, navigate to the 'Plot' page where the 'One-Time' and 'Stream' buttons are also accessible to capture the power data. The title of the graph can be changed by clicking on it. The graph also shows all the possible power rails which can be selected/deselected to make the rail visible.
Figure 1-3 Live Graph of AM62L Power Consumption. The AM62L Power Visualizer Tool's captured data outputs are provided as is and are not verified within a specified precision. It should not be used for power supply sizing.