SLUUBD0A September 2015 – January 2026
This section is for single cell gauges that do not update these parameters automatically.
Use the final enclosure of your application/device. The cell needs to be installed in the final enclosure so that the tool can measure the thermal conductivity of the whole system (from cell through the enclosure to ambient temperature). Make sure that the system is NOT exposed to the air-stream of the temperature chamber but instead shield it from a fan so that the cell will heat up as if it were used at the target ambient temperature.
Using this test setup produces the most accurate thermal model parameters but it will not result in accurate RbL values at the target temperature as the cell will heat up, possibly significantly (depending on self-heating: this can exceed a temperature rise of 30°C.)