SLUUBD0A September 2015 – January 2026
Use the bare cell with a thermistor tightly attached to the cell so that the thermistor measures the actual temperature of the cell.
Keep the cell soaked at the target temperature where you require the most accurate resistance. For example -10°C. Make sure that the cell is exposed to the air-stream of the temperature chamber so that any self heating dissipates efficiently. The thermistor should be installed under the cell so that it measures the temperature of the cell and not the forced air from the temperature chamber. The goal is for the cell to be at the target temperature for the optimized RbL table.
Using this test setup produces the most accurate RbL table but it will not result in accurate thermal model parameters because the cell is forced to the target temperature.