SLUAAM6 November 2022 BQ24190 , BQ24192 , BQ24192I , BQ24195 , BQ24195L , BQ24196 , BQ24292I , BQ24295 , BQ24296 , BQ24297 , BQ24298 , BQ25600 , BQ25600D , BQ25601 , BQ25601D , BQ25606 , BQ25611D , BQ25616 , BQ25618 , BQ25619 , BQ25620 , BQ25622 , BQ25890 , BQ25890H , BQ25892 , BQ25895 , BQ25896 , BQ25898 , BQ25898D
This application report provides a general single-cell charge selection guidance and comparison among BQ2419x, BQ2429x, BQ2589x, BQ25898x, BQ2560x, BQ2561x, and BQ2562x single-cell switching battery charge devices with Narrow Voltage DC (NVDC) Power Path Management. The document presents the main differences and describes the key features of each part. The summary also includes the comparison across various charger product families. This information provided hereby can assist design engineers with making good choices for their single-cell switching battery charging applications.
All trademarks are the property of their respective owners.
Besides the common charger parameters such as the input voltage range, the battery charge voltage limit, the maximum charging current, the package size and so on, a single-cell charger designer needs to consider system-level architecture including but not limit to the input current limit detection scheme, the system control methodology, the system monitoring and protection scheme and boost mode operation.
If the application requires USB D+/D- input current limit detection capability, the user needs to check the related specs of a charger IC. Please visit USB D+ D- Input Current Limit Detection for BQ2419x, BQ2429x, BQ2589x, BQ25898x, BQ2560x, and BQ2561x (USB D+ D- Input Current Limit Detection for BQ2419x, BQ2429x, BQ2589x, BQ25898x, BQ2560x, and BQ2561x application note) for the details.
If the application does not require USB D+/D- input current limit, the user can either leave the D+/D- pins open or short the D+/D- pins together. Below are the general guidelines. Please refer to the corresponding data sheet for the specific input current limit settings
As a battery charger designer, one of the most important questions to consider is the control method for the charging system. Shall a microprocessor-controlled charger or a stand-alone charger be used?
The two most popular control methodologies are:
Table 1-1 lists what can be considered when determining the control method for a charger system.
I2C-controlled | Stand-alone | |
---|---|---|
Need real-time control over the charger? | √ | X |
Need the flexibility of charging parameters? | √ | X |
Need to monitor charging parameter values? | √ | X |
Require a host? | Yes | No |
Require software code? | Yes | No |