SLUAAL7 September   2022 BQ35100

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2EVM and System Setup
  5. 3Enabling EOS Mode
    1. 3.1 Steps for Enabling EOS Mode
  6. 4I2C Communication Between the Microcontroller and the BQ35100 EVM
  7. 5Testing Procedure
  8. 6EOS Data Example
  9. 7Final Configuration of the BQ35100 Data
  10. 8Conclusion
  11. 9References

Enabling EOS Mode

Scaled resistance and measured impedance values are only updated when the gauge is in EOS mode. Using BQStudio is the easiest way to configure the gauge to EOS Mode.