SLOS700C January 2011 – April 2016
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
For device support, see the following:
Gerber – http://focus.ti.com/docs/toolsw/folders/print/TPA6139A2evm.html
For related documentation, see the following:
TPA6139A2EVM User's Guide (SLOU308)
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
DirectPath, E2E are trademarks of Texas Instruments.
Blu-ray Discs is a trademark of Blu-ray Disc Association.
All other trademarks are the property of their respective owners.

These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.