SLOS700C January 2011 – April 2016
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPA6139A2 device starts its operation by asserting the MUTE pin to logic 1. The device enters in mute mode when pulling the MUTE pin low. The charge pump generates a negative supply voltage. The charge pump flying capacitor connected between CP and CN transfers charge to generate the negative supply voltage. The output voltages are capable of positive and negative voltage swings and are centered close to 0 V, eliminating the need for output capacitors. Input coupling capacitors block any DC bias from the audio source and ensure maximum dynamic range.
This typical connection diagram highlights the required external components and system level connections for proper operation of the device in popular use case. Any design variation can be supported by TI through schematic and layout reviews. Visit https://e2e.ti.com for design assistance and join the audio amplifier discussion forum for additional information.
The TPA6139A2 has the ability to drive a high capacitive load up to 220 pF directly. Higher capacitive loads can be accepted by adding a series resistor of 47 Ω or larger for the line driver output.
Figure 11. Single-Ended Input and Output, Gain Set to –1.5x
Table 1 lists the design parameters of this example.
| DESIGN PARAMETER | EXAMPLE VALUE |
|---|---|
| Input voltage supply range | 3 V to 3.6 V |
| Current | 130 mA |
| Load impedance | 32 Ω |
The charge pump flying capacitor serves to transfer charge during the generation of the negative supply voltage. The VSS capacitor must be at least equal to the charge pump capacitor in order to allow maximum charge transfer. Low ESR capacitors are an ideal selection, and a value of 1 μF is typical. Capacitor values that are smaller than 1 μF cannot be recommended as it limits the negative voltage swing in low impedance loads.
The TPA6139A2 is a DirectPath amplifier that requires adequate power-supply decoupling to ensure that the noise and total harmonic distortion (THD) are low. A good low equivalent-series-resistance (ESR) ceramic capacitor, typically 1 μF, placed as close as possible to the device VDD leads works best. Placing this decoupling capacitor close to the TPA6139A2 is important for the performance of the amplifier. For filtering lower frequency noise signals, a 10-μF or greater capacitor placed near the audio power amplifier also helps, but it is not required in most applications because of the high PSRR of this device.
The gain setting is programmed with the GAIN pin individually for line driver and headphone section. Gain setting is latched when the MUTE pin is set high. Table 2 lists the gain settings. The default gain with the gain-set pin left open is –2x.
| Gain_set RESISTOR | GAIN | GAIN (dB) | INPUT RESISTANCE |
|---|---|---|---|
| No connect | –2x | 6 | 37k |
| 82k0 | –1x | 0 | 55k |
| 49k2 | –1.5x | 3.5 | 44k |
| 35k1 | –2.3x | 7.2 | 33k |
| 27k3 | –2.5x | 8 | 31k |
| 20k5 | –3x | 9.5 | 28k |
| 15k4 | –3.5x | 10.9 | 24k |
| 11k5 | –4x | 12 | 22k |
| 9k09 | –5x | 14 | 18k |
| 7k50 | –5.6x | 15 | 17k |
| 6k19 | –6.4x | 16.1 | 15k |
| 5k11 | –8.3x | 18.4 | 12k |
| 3k90 | –10x | 20 | 10k |
DC input-blocking capacitors are required to be added in series with the audio signal into the input pins of the TPA6139A2. These capacitors block the DC portion of the audio source and allow the TPA6139A2 inputs to be properly biased to provide maximum performance. The input blocking capacitors also limit the DC gain to 1, limiting the DC-offset voltage at the output.
These capacitors form a high-pass filter with the input resistor, RIN. The cutoff frequency is calculated using Equation 1. For this calculation, the capacitance used is the input-blocking capacitor and the resistance is the input resistor chosen from Table 2. Then the frequency or capacitance can be determined when one of the two values is given, as shown in Equation 1.
For a fixed cutoff frequency of 2 Hz, the size of the input capacitance is shown Table 3 with the capacitors rounded up to the nearest E6 values. For 20-Hz cutoff, simply divide the capacitor values with 10; for example, for 1x gain, 150 nF is needed.
| Gain_set RESISTOR |
GAIN | Gain (dB) |
INPUT RESISTANCE |
2-Hz CUTOFF |
|---|---|---|---|---|
| 249k | –2x | 6 | 37k | 2.2 µF |
| 82k0 | –1x | 0 | 55k | 1.5 µF |
| 49k2 | –1.5x | 3.5 | 44k | 2.2 µF |
| 35k1 | –2.3x | 7.2 | 33k | 3.3 µF |
| 27k3 | –2.5x | 8 | 31k | 3.3 µF |
| 20k5 | –3x | 9.5 | 28k | 3.3 µF |
| 15k4 | –3.5x | 10.9 | 24k | 3.3 µF |
| 11k5 | –4x | 12 | 22k | 4.7 µF |
| 9k09 | –5x | 14 | 18k | 4.7 µF |
| 7k50 | –5.6x | 15 | 17k | 4.7 µF |
| 6k19 | –6.4x | 16.1 | 15k | 6.8 µF |
| 5k11 | –8.3x | 18.4 | 12k | 6.8 µF |
| 3k90 | –10x | 20 | 10k | 10 µF |
The characteristics of this design are shown in Typical Characteristics, Line Driver.