SLAZ722H May   2018  – August 2021 MSP430FR2155

 

  1.   1
  2.   2
  3.   3
  4.   4
  5.   5
    1.     6
    2.     7
      1.      8
      2.      9
      3.      10
      4.      11
    3.     12
  6.   13
    1.     14
    2.     15
    3.     16
    4.     17
    5.     18
    6.     19
    7.     20
    8.     21
    9.     22
    10.     23
    11.     24
    12.     25
    13.     26
  7.   27

EEM23

EEM Module

Category

Debug

Function

EEM triggers incorrectly when modules using wait states are enable; Incorrect operation when more than two software breakpoints are set in the continual instruction addresses

Description

When modules using wait states (USB, MPY, CRC and FRAM controller in manual mode) are enabled, the EEM may trigger incorrectly.  This can lead to an incorrect profile counter value or cause issues with the EEMs data watch point, state storage, and breakpoint functionality.
When more than 2 software breakpoints are set in continuous instruction addresses (for example, more than 2 NOP instructions, the address is increased 2 bytes between these 2 instructions), program counter (PC) will stuck at the first breakpoint and can't move on.

Workaround

None.

Note: This erratum affects debug mode only.