SLASEL0B October 2019 – June 2020
PRODUCTION DATA.
Arbitrary waveform generation circuits are common in memory and semiconductor test equipment. These circuits are used to generate reference ac waveforms to test semiconductor devices. The key performance parameters of such circuits are THD, SNR, and the update rate. Figure 65 shows the basic building block example of an AWG circuit using the DACx1001.
Figure 65. Arbitrary Waveform Generation