SLAK034 December 2024 DAC121S101-SEP
For HDR a step-stress test method was used to determine the TID hardness level and a single test method to determine HDR TID. Prior to and after testing, electrical test were performed on a given sample of parts to verify that the units are within specified data sheet electrical test limits. The RLAT 5 sample units were used at the 50-300 rad(Si)/s dose level with biased setup conditions and this is repeated for each wafer lot.
The tables below list the serialized samples used for RHA characterization.
| HDR = 171 rad(Si)/s |
|---|
| Total Samples: 5 |
| Exposure Levels |
| 30 krad(Si) |
| Biased |
| 22-26 |