SLAAEP3 December 2025 ULC1001
Once the lens cover is properly positioned within the housing, this constitutes the final lens control system (LCS). The housing contributes additional damping, which can result in an increase in the impedance of the lens cover. Make sure to regulate the induced damping from the housing to the smallest extent possible.

Figure 3-6 shows the impedance response of the LCS. Compared to the Lens Cover, the resonant frequency of the 65.8kHz changes to 66.2kHz, which is relatively minimal. The impedance increases significantly from 226.7Ω to 337.6Ω.
Figure 3-6 Impedance Response of LCS