SLAAE46 November   2021 DAC43701

 

  1.   Trademarks
  2. 1Introduction
  3. 2NVM Online Update to Minimize Flicker
  4. 3Application Example
    1. 3.1 Design Note
    2. 3.2 Optimize Power Sequence
    3. 3.3 DAC Pseudo Code Example
  5. 4Summary
  6. 5References

Optimize Power Sequence

In addition, the common-mode voltage range should be considered to avoid the amplifier working in a nonlinear state. The common-mode voltage of the circuit in Figure 1-2 is 0V, and the common-mode voltage range of the OPA2170 is from (VEE-0.1V) to (VCC-2V). As the bias voltage is divided from VEE, if the VEE supply is applied earlier than VCC, the clipping voltage will be observed at the VCOM output as shown in Figure 3-1, which may cause unexpected flicker.

GUID-20211011-SS0I-0WWS-KJ8K-Z85LQ3PJFZ5Z-low.pngFigure 3-1 Transient Simulation Results When VEE Rises up Earlier

To avoid the clipping issue, VCC should power on before VEE, and ensure VCC is greater than 2 V(typical) when VEE powers on, as shown in Figure 3-2.

GUID-20211011-SS0I-BKWN-84MN-WKNJKB5BV617-low.pngFigure 3-2 Transient Simulation Results When VCC Rises up Earlier