SLAA889A March   2019  – July 2021 MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471

 

  1.   Trademarks
  2. 1Flow Metering Background
    1. 1.1 Water Flow Velocity Estimation
      1. 1.1.1 Velocity of Ultrasound in Water is Known
      2. 1.1.2 Velocity of Ultrasound in Water is Unknown
  3. 2Algorithms for Ultrasonic Water Flow Metering
    1. 2.1 Correlation Based Technique for Differential TOF Estimation
    2. 2.2 Absolute Time-of-Flight (AbsTOF) Measurement (Tup and Tdn)
      1. 2.2.1 AbsTOF Calculation
        1. 2.2.1.1 Acquisition Algorithm for AbsTOF
        2. 2.2.1.2 Tracking Algorithm for AbsTOF
  4. 3References
  5. 4Revision History

AbsTOF Calculation

The absolute time of flight (AbsToF) is determined by a two-stage process, namely acquisition and tracking. The acquisition process is implemented when there is no previous memory of the absTOF value (for example during the first signal capture) or when the algorithm detects an anomaly in two consecutive measurements of AbsTOF. The acquisition process algorithm consumes more power, so it is not implemented during each measurement. Instead, the tracking algorithm is implemented during each measurement.