| ISET | 1 | GND | The device reports an error on the ISET pin. | B |
| GND | 2 | OUT0 | The device reports LED open. | B |
| OUT0 | 3 | OUT1 | The LEDs connected to the OUT0 and OUT1 pin cannot perform the
correct brightness. | B |
| OUT1 | 4 | OUT2 | The LEDs connected to the OUT1 and OUT2 pin cannot perform the
correct brightness. | B |
| OUT2 | 5 | OUT3 | The LEDs connected to the OUT2 and OUT3 pin cannot perform the
correct brightness. | B |
| OUT3 | 6 | OUT4 | The LEDs connected to the OUT3 and OUT4 pin cannot perform the
correct brightness. | B |
| OUT4 | 7 | OUT5 | The LEDs connected to the OUT4 and OUT5 pin cannot perform the
correct brightness. | B |
| OUT5 | 8 | OUT6 | The LEDs connected to the OUT5 and OUT6 pin cannot perform the
correct brightness. | B |
| OUT6 | 9 | OUT7 | The LEDs connected to the OUT6 and OUT7 pin cannot perform the
correct brightness. | B |
| OUT7 | 10 | OUT8 | The LEDs connected to the OUT7 and OUT8 pin cannot perform the
correct brightness. | B |
| OUT8 |
11 |
OUT9 |
The LEDs connected to the OUT8 and OUT9 pin cannot
perform the correct brightness. |
B |
| OUT9 |
12 |
OUT10 |
The LEDs connected to the OUT9 and OUT10 pin cannot
perform the correct brightness. |
B |
| OUT10 |
13 |
OUT11 |
The LEDs connected to the OUT10 and OUT11 pin cannot
perform the correct brightness. |
B |
| OUT11 |
14 |
SIN |
There is a communication failure. |
B |
| SIN |
15 |
CLK_I |
There is a communication failure. |
B |
| CLK_I |
16 |
FAULT |
The CLK_I and FAULT pin are both corner pins, the
adjacent-pin short is not applicable. |
D |
| FAULT |
17 |
SOUT |
The device reports fault falsely. |
B |
| SOUT |
18 |
GND |
There is a communication failure. |
B |
| GND |
19 |
OUT12 |
The device reports LED open. |
B |
| OUT12 |
20 |
OUT13 |
The LEDs connected to the OUT12 and OUT13 pin cannot
perform the correct brightness. |
B |
| OUT13 |
21 |
OUT14 |
The LEDs connected to the OUT13 and OUT14 pin cannot
perform the correct brightness. |
B |
| OUT14 |
22 |
OUT15 |
The LEDs connected to the OUT14 and OUT15 pin cannot
perform the correct brightness. |
B |
| OUT15 |
23 |
OUT16 |
The LEDs connected to the OUT15 and OUT16 pin cannot
perform the correct brightness. |
B |
| OUT16 |
24 |
OUT17 |
The LEDs connected to the OUT16 and OUT17 pin cannot
perform the correct brightness. |
B |
| OUT17 |
25 |
OUT18 |
The LEDs connected to the OUT17 and OUT18 pin cannot
perform the correct brightness. |
B |
| OUT18 |
26 |
OUT19 |
The LEDs connected to the OUT18 and OUT19 pin cannot
perform the correct brightness. |
B |
| OUT19 |
27 |
OUT20 |
The LEDs connected to the OUT19 and OUT20 pin cannot
perform the correct brightness. |
B |
| OUT20 |
28 |
OUT21 |
The OUT20 and OUT21 pin are both corner pins, the
adjacent-pin short is not applicable. |
D |
| OUT21 |
29 |
OUT22 |
The LEDs connected to the OUT21 and OUT22 pin cannot
perform the correct brightness. |
B |
| OUT22 |
30 |
OUT23 |
The LEDs connected to the OUT22 and OUT23 pin cannot
perform the correct brightness. |
B |
| OUT23 |
31 |
VCC |
The device reports LED short. |
B |
| VCC |
32 |
ISET |
The VCC and ISET pin are both corner pins, the
adjacent-pin short is not applicable. |
D |