| OUT2 | 1 | OUT3 | The LEDs connected to the OUT2 and OUT3 pin cannot perform the
correct brightness. | B |
| OUT3 | 2 | OUT4 | The LEDs connected to the OUT3 and OUT4 pin cannot perform the
correct brightness. | B |
| OUT4 | 3 | OUT5 | The LEDs connected to the OUT4 and OUT5 pin cannot perform the
correct brightness. | B |
| OUT5 | 4 | OUT6 | The LEDs connected to the OUT5 and OUT6 pin cannot perform the
correct brightness. | B |
| OUT6 | 5 | OUT7 | The LEDs connected to the OUT6 and OUT7 pin cannot perform the
correct brightness. | B |
| OUT7 | 6 | OUT8 | The LEDs connected to the OUT7 and OUT8 pin cannot perform the
correct brightness. | B |
| OUT8 | 7 | OUT9 | The LEDs connected to the OUT8 and OUT9 pin cannot perform the
correct brightness. | B |
| OUT9 | 8 | OUT10 | The OUT9 and OUT10 pin are both corner pins, the adjacent-pin short
is not applicable. | D |
| OUT10 | 9 | OUT11 | The LEDs connected to the OUT10 and OUT11 pin cannot perform the
correct brightness. | B |
| OUT11 | 10 | SIN | There is a communication failure. | B |
| SIN |
11 |
CLK_I |
There is a communication
failure. |
B |
| CLK_I |
12 |
FAULT |
The device reports fault
falsely. |
B |
| FAULT |
13 |
SOUT |
The device reports fault
falsely. |
B |
| SOUT |
14 |
GND |
There is a communication
failure. |
B |
| GND |
15 |
OUT12 |
The device reports LED open. |
B |
| OUT12 |
16 |
OUT13 |
The OUT12 and OUT13 pin are both corner
pins, the adjacent-pin short is not applicable. |
D |
| OUT13 |
17 |
OUT14 |
The LEDs connected to the OUT13 and
OUT14 pin cannot perform the correct brightness. |
B |
| OUT14 |
18 |
OUT15 |
The LEDs connected to the OUT14 and
OUT15 pin cannot perform the correct brightness. |
B |
| OUT15 |
19 |
OUT16 |
The LEDs connected to the OUT15 and
OUT16 pin cannot perform the correct brightness. |
B |
| OUT16 |
20 |
OUT17 |
The LEDs connected to the OUT16 and
OUT17 pin cannot perform the correct brightness. |
B |
| OUT17 |
21 |
OUT18 |
The LEDs connected to the OUT17 and
OUT18 pin cannot perform the correct brightness. |
B |
| OUT18 |
22 |
OUT19 |
The LEDs connected to the OUT18 and
OUT19 pin cannot perform the correct brightness. |
B |
| OUT19 |
23 |
OUT20 |
The LEDs connected to the OUT19 and
OUT20 pin cannot perform the correct brightness. |
B |
| OUT20 |
24 |
OUT21 |
The OUT20 and OUT21 pin are both corner
pins, the adjacent-pin short is not applicable. |
D |
| OUT21 |
25 |
OUT22 |
The LEDs connected to the OUT21 and
OUT22 pin cannot perform the correct brightness. |
B |
| OUT22 |
26 |
OUT23 |
The LEDs connected to the OUT22 and
OUT23 pin cannot perform the correct brightness. |
B |
| OUT23 |
27 |
VCC |
The device reports LED short. |
B |
| VCC |
28 |
ISET |
The device reports an error on the ISET
pin. |
B |
| ISET |
29 |
GND |
The device reports an error on the ISET
pin. |
B |
| GND |
30 |
OUT0 |
The device reports LED open. |
B |
| OUT0 |
31 |
OUT1 |
The LEDs connected to the OUT0 and OUT1
pin cannot perform the correct brightness. |
B |
| OUT1 |
32 |
OUT2 |
The OUT1 and OUT2 pin are both corner
pins, the adjacent-pin short is not applicable. |
D |