SFFSAX8 December 2025 LMH6551Q-Q1
This section provides a failure mode analysis (FMA) for the pins of the LMH6551Q-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the LMH6551Q-Q1 pin diagram. For a detailed description of the device pins please refer to the Connection Diagram section in the LMH6551Q-Q1 datasheet.
Figure 4-1 Pin DiagramFollowing are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN- | 1 | An input at mid-supply (GND) is a valid input; however, the desired result for the application is unlikely. | C |
| VCM | 2 | The device operates as normal, unless a single supply voltage is intended. | D |
| V+ | 3 | The diodes from the input to the V+ pin potentially turn on due to an input signal and this results in electrical overstress (EOS). | A |
| +OUT | 4 | The device potentially overheats. | B |
| -OUT | 5 | The device potentially overheats. | B |
| V- | 6 | The diodes from the input to the V- pin potentially turn on due to an input signal and cause electrical overstress (EOS). The device operates as normal if a single supply configuration is used. | A |
| NC | 7 | The device operates as normal. The pin has no internal connection. | D |
| IN+ | 8 | An input at mid-supply (GND) is a valid input; however, the desired result for the application is unlikely. | C |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN- | 1 | The input is floating, the circuit potentially does not function as expected. | C |
| VCM | 2 | The device operates as normal. The output common-mode is set to mid-supply. | D |
| V+ | 3 | The output pin with the highest voltage tries to power the V+ pin of the device. | B |
| OUT+ | 4 | The output can be left open. There is no effect on the device, but the output is not measured. | C |
| OUT- | 5 | The output can be left open. There is no effect on the device, but the output is not measured. | C |
| V- | 6 | The output pin with the lowest voltage tries to power the V- pin of the device. | B |
| NC | 7 | The device operates as normal. The NC pin has no internal connection. | D |
| IN+ | 8 | There input is floating, the circuit likely does not function as expected. | C |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| 1 | IN- | VCM | Tying the input pin to the VCM pin is valid; however, the desired result for the application is unlikely. | C |
| 2 | VCM | V+ | Tying the VCM pin to the V+ pin is valid; however, the desired result for the application is unlikely. | C |
| 3 | V+ | OUT+ | Tying the V+ pin to the output pin is valid; however, the desired result for the application is unlikely. | C |
| 4 | OUT+ | OUT- | TI does not recommend tying the output pin to the other output pin; the desired result for the application is unlikely, the device potentially overheats and damage occurs. The pins are separated across the device package. | B |
| 5 | OUT- | V- | Tying the output pin to the V- pin is valid; however, the desired result for the application is unlikely. | C |
| 6 | V- | NC | The device operates as normal. The NC pin has no internal connection. | D |
| 7 | NC | IN- | The device operates as normal. The NC pin has no internal connection. | D |
| 8 | IN+ | IN- | TI does not recommend tying the input pin to the other input pin; the desired result for the application is unlikely, the device potentially overheats and damage occurs. The pins are separated across the device package. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| NC | 7 | The device operates as normal. The NC pin has no internal connection. | D |
| IN- | 1 | Input at V+ is a valid input; however, the desired result for the application is unlikely. | C |
| OUT+ | 4 | The device potentially overheats. | B |
| VCM | 2 | Tying the VCM pin at the V+ pin is a valid input; however, the desired result for the application is unlikely. | C |
| V+ | 3 | The device operates as normal. | D |
| OUT- | 5 | The device potentially overheats. | B |
| IN+ | 8 | Input at V+ is a valid input; however, the desired result for the application is unlikely. | C |
| V- | 6 | The diodes from input to the V- pin potentially turn on due to an input signal and this results in electrical overstress (EOS). | A |