SFFSAW9A November 2025 – December 2025 LM65680
This section provides a failure mode analysis (FMA) for the pins of the LM65640, LM65660, and LM65680. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the LM65640, LM65660, and LM65680 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LM656X0 datasheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| NC | 1 | The device operates as normal. | D |
| 11 | |||
| 13 | |||
| 15 | |||
| 20 | |||
| 22 | |||
| PG | 2 | There is a loss of Power Good functionality. | B |
| COMP | 3 | When there is internal compensation, the device operates as normal. | D |
| When there is external compensation, there is a loss of regulation. VOUT = 0V. | B | ||
| FB | 4 | When VOUT is fixed at 3.3V, the FB pin is shorted to ground by default. The device operates as normal. | D |
| When VOUT is fixed at 5V, the VCC pin shorts to ground. There is a loss of regulation. VOUT = 0V. | B | ||
| When VOUT is adjustable, there is a loss of regulation. VOUT = VIN. | B | ||
| SS | 5 | There is a loss of regulation. VOUT = 0V. | B |
| SGND | 6 | The device operates as normal. | D |
| CNFG/SYNCOUT | 7 | There is a loss of regulation. VOUT = 0V. | B |
| MODE/SYNC | 8 | In AUTO mode, the device operates as normal. | D |
| In FPWM mode, there is a loss of regulation. VOUT = 0V. | B | ||
| In external SYNC, there is a loss of synchronization. The performance of the device degrades. The device operates in AUTO mode. | C | ||
| RT | 9 | When the frequency is fixed at 400kHz, there is a loss of regulation. VOUT = 0V. | B |
| When the frequency is fixed at 2.2MHz, the device operates as normal. | D | ||
| When the frequency is adjustable, the performance of the device degrades. The device switches at 2.2MHz. | C | ||
| EN/UVLO | 10 | The device disables. VOUT = 0V. | D |
| PGND1, PGND2 | 12 | The device operates as normal. | D |
| 23 | |||
| VIN1, VIN2 | 14 | VOUT = 0V. | B |
| 21 | |||
| SW1, SW2, SW3 | 16 | The device is damaged. | A |
| 17 | |||
| 18 | |||
| BST | 19 | There is a loss of regulation. VOUT = 0V. | B |
| VCC | 24 | There is a loss of regulation. VOUT = 0V. | B |
| DRSS/MCOMM | 25 | The DRSS pin is disabled. Slew rate control is disabled. The performance of EMI degrades. | C |
| BIAS | 26 | When the BIAS pin is tied to VOUT, there is a loss of regulation. VOUT = 0V. | B |
| When the BIAS pin is tied to ground, the device operates as normal. | D |
| Pin Name | Pin No | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| NC | 1 | The device operates as normal. | D |
| 11 | |||
| 13 | |||
| 15 | |||
| 20 | |||
| 22 | |||
| PG | 2 | There is a loss of Power Good functionality. | B |
| COMP | 3 | When there is internal compensation, the device operates as normal. | D |
| When there is external compensation, the performance of the device degrades. | C | ||
| FB | 4 | When VOUT is fixed, there is a loss of regulation. VOUT = 0V. | B |
| When VOUT is adjustable, there is a loss of regulation. VOUT = VIN. | B | ||
| SS | 5 | The device operates as normal. | D |
| SGND | 6 | The performance of the device degrades. | C |
| CNFG/SYNCOUT | 7 | There is a loss of regulation. VOUT = 0V. | B |
| MODE/SYNC | 8 | In AUTO mode, the device operates as normal. | D |
| In FPWM mode, the AUTO operation occurs in the next cycle. The performance of the device degrades. | C | ||
| In external SYNC, there is a loss of synchronization. The device operates in AUTO mode. The performance of the device degrades. | C | ||
| RT | 9 | When the frequency is fixed at 400kHz, the performance of the device degrades. The device operates at 2.2MHz. | C |
| When the frequency is fixed at 2.2MHz, the device operates as normal. | D | ||
| When the frequency is adjustable, the performance of the device degrades. The device operates at 2.2MHz. | C | ||
| EN/UVLO | 10 | The device disables. VOUT = 0V. | B |
| PGND1, PGND2 | 12 | The degradation in performance depends on the conditions of the application. | C |
| 23 | |||
| VIN1, VIN2 | 14 | The degradation in performance depends on the conditions of the application. | C |
| 21 | |||
| SW1, SW2, SW3 | 16 | The degradation in performance depends on the conditions of the application. | C |
| 17 | |||
| 18 | |||
| BST | 19 | There is a loss of regulation. VOUT = 0V. | B |
| VCC | 24 | The LDO operation is unstable. There is a loss of regulation. | B |
| DRSS/MCOMM | 25 | The DRSS pin is enabled. The slew rate control is enabled. The device operates as normal. | D |
| BIAS | 26 | When VOUT is fixed, there is a loss of regulation. VOUT = 0V. | B |
| When VOUT is adjustable, the performance of the device degrades. The IQ is higher. | C |
| Pin Name | Adjacent Pin | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| NC | PG | The device operates as normal. | D |
| PG | COMP | When there is internal compensation, there is a loss of PG functionality. | B |
| When there is external compensation, there is a loss of regulation. | B | ||
| COMP | FB | When there is external compensation, and VOUT is fixed at 3.3V, there is a loss of regulation. VOUT = 0. | B |
| When there is external compensation, and VOUT is fixed at 5V, there is a loss of regulation. There is an overvoltage condition. | B | ||
| When there is external compensation, and VOUT is adjustable, there is a loss of regulation. There is an overvoltage condition. | B | ||
| FB | SS | When VOUT is fixed at 3.3V, there is a loss of regulation. VOUT = 0. | B |
| When VOUT is fixed at 5V, there is a loss of regulation. VOUT = 0. | B | ||
| When VOUT is adjustable, there is a loss of regulation. | B | ||
| SS | SGND | There is a loss of regulation. VOUT = 0V. | B |
| SGND | CNFG/SYNCOUT | There is a loss of regulation. VOUT = 0V. | B |
| CNFG/SYNCOUT | MODE/SYNC | When there is internal compensation (COMP pin tied to VCC), the device operates in FPWM mode. | D |
| When there is external compensation (COMP pin pulled to GND with a 49.9kΩ resistor), the device operates in AUTO mode. | D | ||
| MODE/SYNC | RT | The RT pin is tied to GND and the MODE pin is tied to GND. The device operates as normal. | D |
| The RT pin is tied to GND and the MODE pin is tied to VCC. There is a loss of regulation. VOUT = 0. | B | ||
| The RT pin is tied to VCC and the MODE pin is tied to GND. There is a loss of regulation. VOUT = 0. | B | ||
| The RT pin is tied to VCC and the MODE pin is tied to VCC. The device operates as normal. | D | ||
| The RT pin is pulled to GND with a resistor and the MODE pin is tied to GND. There is a loss of regulation. | B | ||
| The RT pin is pulled to GND with a resistor and the MODE pin is tied to VCC. There is a loss of regulation. | B | ||
| RT | EN/UVLO | The RT pin is tied to GND and the EN pin is tied to VIN. There is a loss of regulation. VOUT = 0. | B |
| The RT pin is tied to VCC and the EN pin is tied to VIN. The device is damaged. | A | ||
| The RT pin is pulled to GND with a resistor and the EN pin is tied to VIN. The performance of the device degrades. | C | ||
| EN/UVLO | NC | The device operates as normal. | D |
| NC | PGND1 | The device operates as normal. | D |
| PGND1 | NC | The device operates as normal. | D |
| NC | VIN1 | The device operates as normal. | D |
| VIN1 | NC | The device operates as normal. | D |
| NC | SW1 | The device operates as normal. | D |
| SW1 | SW2 | The device operates as normal. | D |
| SW2 | SW3 | The device operates as normal. | D |
| SW3 | BST | The device operates as normal. | B |
| BST | NC | The device operates as normal. | D |
| NC | VIN2 | The device operates as normal. | D |
| VIN2 | NC | The device operates as normal. | D |
| NC | PGND2 | The device operates as normal. | D |
| PGND2 | VCC | There is a loss of regulation. VOUT = 0V. | B |
| VCC | DRSS/MCOMM | The DRSS pin is tied to VCC. The device operates as normal. | D |
| The DRSS pin is tied to GND. There is a loss of regulation. VOUT = 0V. | B | ||
| The DRSS pin is pulled to GND with a resistor. The performance of the device degrades. | C | ||
| DRSS/MCOMM | BIAS | The DRSS pin is tied to GND and the BIAS pin is tied to GND. The device operates as normal. | D |
| The DRSS pin is tied to VCC and the BIAS pin is tied to GND. There is a loss of regulation. VOUT = 0V. | B | ||
| The DRSS pin is pulled to GND with a resistor and the BIAS pin is tied to GND. The performance of the device degrades. | C | ||
| The DRSS pin is tied to GND and the BIAS pin is tied to VOUT. There is a loss of regulation. | B | ||
| The DRSS pin is tied to VCC and the BIAS pin is tied to VOUT (<5V). The device operates as normal. | D | ||
| The DRSS pin is tied to VCC and the BIAS pin is tied to VOUT (>5V). The device is damaged. | A | ||
| The DRSS pin is pulled to GND with a resistor and the BIAS pin is tied to VOUT. The performance of the device degrades. | C | ||
| BIAS | NC | The device operates as normal. | D |
| Pin Name | Pin No | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| NC | 1 | The device operates as normal. | D |
| 11 | |||
| 13 | |||
| 15 | |||
| 20 | |||
| 22 | |||
| PG | 2 | The device is damaged if supply > Absolute Maximum Rating. | A |
| COMP | 3 | The device is damaged if supply > 5.5V. | A |
| FB | 4 | The device is damaged if supply > 5.5V. | A |
| SS | 5 | The device is damaged if supply > 5.5V. | A |
| SGND | 6 | VOUT = 0V. | B |
| CNFG/SYNCOUT | 7 | The device is damaged if supply > 5.5V. | A |
| MODE/SYNC | 8 | The device is damaged if supply > 5.5V. | A |
| RT | 9 | The switching frequency is undefined. The performance of the device degrades. | C |
| EN/UVLO | 10 | The device operates as normal. | D |
| PGND1, PGND2 | 12 | VOUT = 0V. | B |
| 23 | |||
| VIN1, VIN2 | 14 | The device operates as normal. | D |
| 21 | |||
| SW1, SW2, SW3 | 16 | The device is damage. | A |
| 17 | |||
| 18 | |||
| BST | 19 | The device is damage. | A |
| VCC | 24 | The device is damaged if supply > 5.5V. | A |
| DRSS/MCOMM | 25 | The device is damaged if supply > Absolute Maximum Rating. | A |
| BIAS | 26 | The device is damaged if supply > Absolute Maximum Rating. | A |