SFFSAU9 December 2025 TPS1HC08-Q1
This section provides a failure mode analysis (FMA) for the pins of the TPS1HC08-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the TPS1HC08-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS1HC08-Q1 datasheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VOUT | 1 | The current limit of the device engages, and thermal protection turns off the FET. | B |
| 11 | |||
| VBB | 2 | The output stages are not powered, and the FET does not turn ON. | B |
| ILIM | 3 | The current limit is set at a maximum level, as per the datasheet. | C |
| GND | 4 | Any GND network, connected for protection, is bypassed. | B |
| NC | 5 | There is no effect on the device. | D |
| 8 | |||
| DIAG_EN | 6 | The diagnostic features do not function, including current sense and fault reporting. | B |
| EN | 7 | The FET is turned off and reports an erroneous open-load fault for no-load conditions when the DIAG_EN pin is high. | B |
| SNS | 9 | The reported SNS current or fault status on the SNS pin is erroneous. | B |
| FLT | 10 | The reported fault status is potentially erroneous. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VOUT | 1 | During the ON state of the device, FET is disconnected. During the OFF state of the device, if the DIAG_EN pin is high, an open-load fault reports. | B |
| 11 | |||
| VBB | 2 | The device is not powered and the FET is kept OFF. | B |
| ILIM | 3 | The current limit is set at a minimum level, as per the datasheet. | C |
| GND | 4 | The loss of ground detection engages, and the device turns OFF. | B |
| NC | 5 | There is no effect on the device. | D |
| 8 | |||
| DIAG_EN | 6 | The diagnostic features do not function, including current sense and fault reporting. (internal pulldown). | B |
| EN | 7 | The FET is turned off and reports an erroneous open-load fault for no-load conditions when the DIAG_EN pin is high. (internal pulldown). | B |
| SNS | 9 | The current sense and fault at the SNS pin is not reported. | B |
| FLT | 10 | The fault condition is not reported. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| VOUT | 1 | VBB | The output is pulled to supply voltage. A short-to-battery detection triggers during the OFF state if the DIAG_EN pin is high. | B |
| 11 | ||||
| ILIM | 3 | VBB | There is a loss of the current limit setting based on the RLIM resistor. | C |
| GND | 4 | ILIM | The current limit is set at a maximum level, as per the datasheet. | C |
| NC | 5 | GND | There is no effect on the device. | D |
| DIAG_EN | 6 | NC | There is no effect on the device. | D |
| EN | 7 | DIAG_EN | Loss of enable control and open-load fault detection is erroneous when the DIAG_EN pin is high. | B |
| NC | 8 | EN | There is no effect on the device. | D |
| SNS | 9 | NC | There is no effect on the device. | D |
| FLT | 10 | SNS | The reported fault status and voltage of the SNS pin is potentially erroneous. | B |
| VBB | 2 | FLT | The reported fault status is potentially erroneous. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VOUT | 1 | The output of FET is pulled to the supply voltage. A short-to-battery detection triggers during the OFF state if the DIAG_EN pin is high. | B |
| 11 | |||
| VBB | 2 | There is no effect on the device. | D |
| ILIM | 3 | There is a loss of the current limit setting based on the RLIM resistor. | C |
| GND | 4 | The supply power is bypassed, and the device stays OFF. | B |
| NC | 5 | There is no effect on the device. | D |
| 8 | |||
| DIAG_EN | 6 | There is a potential violation of the absolute maximum rating for the pin and a possible breakdown of the ESD cell. | A |
| EN | 7 | There is a potential violation of the absolute maximum rating for the pin and a possible breakdown of the ESD cell. | A |
| SNS | 9 | There is a potential violation of the absolute maximum rating for the pin and a possible breakdown of the ESD cell. | A |
| FLT | 10 | The reported fault status is potentially erroneous. | B |