SFFSAU5A March 2026 – May 2026 UCC27624V-Q1
This section provides a failure mode analysis (FMA) for the pins of the UCC27624V-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1, Figure 4-2, Figure 4-3, and Figure 4-4 show the UCC27624V-Q1 pin diagrams. For a detailed description of the device pins, see the Pin Configuration and Functions section in the UCC27624V-Q1 datasheet.
Figure 4-1 D Package Pin DiagramFollowing are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| ENA | 1 | The function of the ENA pin is disabled. The OUTA pin does not respond to the INA pin. | B |
| INA | 2 | The function of the INA pin is lost. The OUTA pin is stuck low. | B |
| GND | 3 | There is no impact on the device. | D |
| INB | 4 | The function of the INB pin is lost. The OUTB pin is stuck low. | B |
| OUTB | 5 | The OUTB pin is stuck low. The OUTB pin is short circuited if the INB pin is commanded High. | A |
| VDD | 6 | There is an undervoltage of the VDD pin. The OUTA and OUTB pins are off. | B |
| OUTA | 7 | The OUTA pin is stuck low. The OUTA pin is short circuited if the INA pin is commanded High. | A |
| ENB | 8 | The function of the ENB pin is disabled. The OUTB pin does not respond to the INB pin. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| ENA | 1 | The OUTA pin is always enabled. The OUTA pin responds to the INA pins. | B |
| INA | 2 | The function of the INA pin is lost. The OUTA pin is stuck low. | B |
| GND | 3 | The state of the OUTA and OUTB pins are unknown. | B |
| INB | 4 | The function of the INB pin is lost. The OUTB pin is stuck low. | B |
| OUTB | 5 | The OUTB pin is disconnected from the power FET. | B |
| VDD | 6 | There is an undervoltage of the VDD pin. The OUTA and OUTB pins are off. | B |
| OUTA | 7 | The OUTA pin is disconnected from the power FET. | B |
| ENB | 8 | The OUTB pin is always enabled. The OUTB pin responds to the INB pin. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| ENA | 1 | INA | The ENA pin cannot override the command of the INA pin. The OUTA pin responds to the INA pin. | B |
| INA | 2 | GND | The OUTA pin is stuck low. | B |
| GND | 3 | INB | The OUTB pin is stuck low. | B |
| OUTB | 5 | VDD | The OUTB pin is stuck high. | A |
| VDD | 6 | OUTA | The OUTA pin is stuck high. | A |
| OUTA | 7 | ENB | The function of the ENB pin depends on the state of the INA (OUTA) pin. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| ENA | 1 | The OUTA pin is always enabled. The OUTA pin responds to the INA pin. | B |
| INA | 2 | The OUTA pin is stuck high. | B |
| GND | 3 | The power supply is short circuited. | B |
| INB | 4 | The OUTB pin is stuck high. | B |
| OUTB | 5 | The OUTB pin is stuck high. | A |
| VDD | 6 | There is no impact on the device. | D |
| OUTA | 7 | The OUTA pin is stuck high. | A |
| ENB | 8 | The OUTB pin is always enabled. The OUTB pin responds to the INB pin. | B |