SFFSAU5A March   2026  – May 2026 UCC27624V-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 D and DDA Package
    2. 2.2 DGN and DGK Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the UCC27624V-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1, Figure 4-2, Figure 4-3, and Figure 4-4 show the UCC27624V-Q1 pin diagrams. For a detailed description of the device pins, see the Pin Configuration and Functions section in the UCC27624V-Q1 datasheet.

UCC27624V-Q1 D Package Pin DiagramFigure 4-1 D Package Pin Diagram
Figure 4-2 DGN Package Pin Diagram
Figure 4-3 DDA Package Pin Diagram
Figure 4-4 DGK Package Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • Pin 1 shorted to pin 8, and pin 4 shorted to pin 5, are not considered.
  • The case of a short-circuit to supply is analyzed as a short to VDD.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
ENA1The function of the ENA pin is disabled. The OUTA pin does not respond to the INA pin.B
INA2The function of the INA pin is lost. The OUTA pin is stuck low.B
GND3There is no impact on the device.D
INB4The function of the INB pin is lost. The OUTB pin is stuck low.B
OUTB5The OUTB pin is stuck low. The OUTB pin is short circuited if the INB pin is commanded High.A
VDD6There is an undervoltage of the VDD pin. The OUTA and OUTB pins are off.B
OUTA7The OUTA pin is stuck low. The OUTA pin is short circuited if the INA pin is commanded High.A
ENB8The function of the ENB pin is disabled. The OUTB pin does not respond to the INB pin.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
ENA1The OUTA pin is always enabled. The OUTA pin responds to the INA pins.B
INA2The function of the INA pin is lost. The OUTA pin is stuck low.B
GND3The state of the OUTA and OUTB pins are unknown.B
INB4The function of the INB pin is lost. The OUTB pin is stuck low.B
OUTB5The OUTB pin is disconnected from the power FET.B
VDD6There is an undervoltage of the VDD pin. The OUTA and OUTB pins are off.B
OUTA7The OUTA pin is disconnected from the power FET.B
ENB8The OUTB pin is always enabled. The OUTB pin responds to the INB pin.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
ENA1INAThe ENA pin cannot override the command of the INA pin. The OUTA pin responds to the INA pin.B
INA2GNDThe OUTA pin is stuck low.B
GND3INBThe OUTB pin is stuck low.B
OUTB5VDDThe OUTB pin is stuck high.A
VDD6OUTAThe OUTA pin is stuck high.A
OUTA7ENBThe function of the ENB pin depends on the state of the INA (OUTA) pin.B
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
ENA1The OUTA pin is always enabled. The OUTA pin responds to the INA pin.B
INA2The OUTA pin is stuck high.B
GND3The power supply is short circuited.B
INB4The OUTB pin is stuck high.B
OUTB5The OUTB pin is stuck high.A
VDD6There is no impact on the device.D
OUTA7The OUTA pin is stuck high.A
ENB8The OUTB pin is always enabled. The OUTB pin responds to the INB pin.B