SFFSAM7A November   2025  – November 2025 TPS62A2N4-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPS62A204-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the TPS62A204-Q1 pin diagram. For a detailed description of the device pins, please refer to the Pin Configuration and Functions section in the TPS62A204-Q1 data sheet.

TPS62A204-Q1 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The device is operating in the typical application. Please refer to the Simplified Schematics in the TPS62A204-Q1 datasheet.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
CONF1There is a loss of functionality. There is the potential for wrong compensation, frequency, and SSC settings.B
VSET2The device powers up with the wrong output voltage.B
SW3The device is potentially damaged.A
4
PG5There is no damage to the device, but loss of functionality occurs.B
VOS6There is no damage to the device, but loss of functionality occurs.B
AGND7There device functions as intended.D
PGND8There device functions as intended.D
13
VIN9The device does not power up.B
10
EN11The device does not power up.B
MODE/SYNC12The device always operates in automatic (auto) mode (PFM/PWM); rather than adjusting the mode to the correct setting.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
CONF 1 There is a loss of functionality. There is the potential for wrong compensation, frequency, and SSC settings. B
VSET 2 The device powers up with the wrong output voltage. B
SW 3 The device powers up and operates if either the 3 or 4 pin is still connected. The performance parameters are potentially degraded. C
4
PG 5 There is no damage to the device, but loss of functionality occurs. B
VOS 6 There is no damage to the device, but the output voltage can be out of regulation. B
AGND 7 The device powers up. C
PGND 8 The device powers up and operates if either the 8 or 13 pin is still connected. The performance parameters are potentially degraded. C
13
VIN 9 The device powers up and operates if either the 9 or 10 pin is still connected. The performance parameters are potentially degraded. C
10
EN 11 If the device is not intended to be disabled, the device does not power up. B
MODE/SYNC 12 The device powers and operates either in FPWM or PFM mode. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
CONF1VSETThere is a loss of functionality. There is the potential for wrong compensation, frequency, and SSC settings.B
VSET2SWThe device powers up but potentially regulates to the wrong output voltage.B
SW3PGThe device is potentially damaged.A
4
PG5VOSThere is a loss of PG functionality.B
VOS6AGNDThere is no damage to the device, but the output voltage can be out of regulation.B
AGND7PGNDThe device powers up and performance parameters are potentially degraded.C
PGND8VINThe device does not power up.B
13
VIN9ENThe device is always enabled.B
10
EN11MODE/SYNCThe device always runs in FPWM mode.B
MODE/SYNC12CONFThe device powers up and operates in either Auto or FPWM mode. There is the potential for wrong compensation, frequency, and SSC settings.B
Table 4-5 Pin FMA for Device Pins Short-Circuited to VIN
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
FSET
CONF1There is a loss of functionality. There is the potential for wrong compensation, frequency, and SSC settings.B
VSET2The device powers up but potentially regulates to the wrong output voltage.B
SW3The device is potentially damaged.A
4
PG5The device is potentially damaged.A
VOS6The output voltage can be out of regulation; the device is potentially damaged.A
AGND7The device does not power up.B
PGND8The device does not power up.B
13
VIN9The device functions as intended.D
10
EN11The device is always enabled, but there is a loss of functionality.B
MODE/SYNC12The device always operates in automatic (auto) mode (PFM/PWM); rather than adjusting the mode to the correct setting.B