SFFS277 November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
CLA doesn’t have an independent watchdog of its own. Hence, it is recommended to perform liveness check periodically by the CPU. Typically, sequential set of events is used to trigger the watchdog (for example, completion of CPU Task1, CLA Task1, CPU Task2, and CLA Task2). The output of the CLA liveness check can be used as one of the tasks to decide the watchdog triggering as indicated in Figure 6-1. The liveness check can be based on application-specific parameters as illustrated in the VDA Egas concept [6] to improve the diagnostic coverage.
Figure 6-1 CLA Liveness Check