SFFS177 October 2021 TCAN1046A-Q1 , TCAN1046AV-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the TCAN1046A-Q1 and TCAN1046AV-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-8 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality |
| B | No device damage, but loss of functionality |
| C | No device damage, but performance degradation |
| D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the TCAN1046A-Q1 pin diagram , and Figure 4-3 shows the TCAN1046AV-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TCAN1046A-Q1/TCAN1046AV-Q1 data sheet.
Figure 4-3 TCAN1046AV-Q1 D Package, 14 Pin
SOIC, Top View
Figure 4-4 TCAN1046AV-Q1 DMT Package, 14 Pin
VSON, Top ViewFollowing are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. (TCAN1046A-Q1) | Pin No. (TCAN1046AV-Q1) | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| TXD1 | 1 | 1 | CAN1 will enter dominant time out mode. Unable to transmit data to the CAN1 bus. | B |
| GND1 | 2 | 2 | None | D |
| VCC1 | 3 | - | CAN1 unpowered, high ICC current. | B |
| VCC | - | 3 | Device unpowered, high ICC current. | B |
| RXD1 | 4 | 4 | RXD default is high side FET ON, with pin short to ground, it forms direct path between supply and ground causing high current | A |
| TXD2 | 5 | 6 | CAN2 will enter dominant time out mode. Unable to transmit data to the CAN2 bus. | B |
| GND2 | 6 | 5 | None | D |
| VCC2 | 7 | - | CAN2 unpowered, high ICC current. | B |
| RXD2 | 8 | 7 | RXD default is high side FET ON, with pin short to ground, it forms direct path between supply and ground causing high current | A |
| CANL2 | 9 | 9 | VO(REC) spec violated. Degraded EMC performance on CAN2 bus. | C |
| CANH2 | 10 | 10 | Device cannot drive dominant to CAN2 bus, no communication possible. | B |
| STB2 | 11 | 8 | STB2 stuck low, CAN2 bus unable to enter low-power mode. | B |
| VIO | - | 11 | Device will be in protected mode. Transceiver passive on both CAN1 and CAN2 bus. | B |
| CANL1 | 12 | 12 | VO(REC) spec violated. Degraded EMC performance on CAN1 bus. | C |
| CANH1 | 13 | 13 | Device cannot drive dominant to CAN1 bus, no communication possible. | B |
| STB1 | 14 | 14 | STB1 stuck low, CAN1 bus unable to enter low-power mode. | B |
| Thermal Pad | - | - | None | D |
| Pin Name | Pin No. (TCAN1046A-Q1) | Pin No. (TCAN1046AV-Q1) | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| TXD1 | 1 | 1 | TXD1 pin defaults high, CAN1 bus state always recessive and unable to transmit data to CAN1 bus. | B |
| GND1 | 2 | 2 | CAN1 unpowered. | B |
| VCC1 | 3 | - | CAN1 unpowered. | B |
| VCC | - | 3 | Device unpowered. | B |
| RXD1 | 4 | 4 | No RXD1 output, unable to receive data from CAN1 bus. | B |
| TXD2 | 5 | 6 | TXD2 pin defaults high, CAN2 bus state always recessive and unable to transmit data to CAN2 bus. | B |
| GND2 | 6 | 5 | CAN2 unpowered. | B |
| VCC2 | 7 | - | CAN2 unpowered. | B |
| RXD2 | 8 | 7 | No RXD2 output, unable to receive data from CAN2 bus. | B |
| CANL2 | 9 | 9 | Device cannot drive dominant on CAN2 bus, unable to communicate. | B |
| CANH2 | 10 | 10 | Device cannot drive dominant on CAN2 bus, unable to communicate. | B |
| STB2 | 11 | 8 | STB2 pin defaults high, CAN2 portion stuck in low-power mode. | B |
| VIO | - | 11 | Device will be in protected mode, Transceiver passive on both CAN1 and CAN2 bus. | B |
| CANL1 | 12 | 12 | Device cannot drive dominant on CAN1 bus, unable to communicate. | B |
| CANH1 | 13 | 13 | Device cannot drive dominant on CAN1 bus, unable to communicate. | B |
| STB1 | 14 | 14 | STB1 pin defaults high, CAN1 portion stuck in low-power mode. | B |
| Thermal Pad | - | - | None | D |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| TXD1 | 1 | GND1 | CAN1 bus will enter dominant time out mode. Unable to transmit data to CAN1 bus. | B |
| GND1 | 2 | VCC1 | CAN1 unpowered, high ICC current. | B |
| VCC1 | 3 | RXD1 | RXD1 output stuck high, unable to receive data from CAN1 bus. | B |
| RXD1 | 4 | TXD2 | RXD1 output reflects the input to TXD2, a separate CAN transceiver. Information from CAN1 will not be received correctly. | B |
| TXD2 | 5 | GND2 | CAN2 bus will enter dominant time out mode. Unable to transmit data to CAN2 bus. | B |
| GND2 | 6 | VCC2 | CAN2 unpowered, high ICC current. | B |
| RXD2 | 8 | CANL2 | Messages on RXD2 will be corrupted by CANL2. Reception of data from CAN2 bus will not be possible. IOS current may be reached. | B |
| CANL2 | 9 | CANH2 | CAN2 bus stuck recessive, no communication possible. IOS current may be reached. | B |
| CANH2 | 10 | STB2 | CAN2 driver and receiver turn off when a dominant is driven on CAN2 bus. May not enter normal mode. | B |
| STB2 | 11 | CANL1 | CAN2 driver and receiver may turn off when the CAN1 bus is recessive. May not enter normal mode. | B |
| CANL1 | 12 | CANH1 | CAN1 bus stuck recessive, no communication possible IOS current may be reached. | B |
| CANH1 | 13 | STB1 | CAN1 driver and receiver turn off when a dominant is driven on CAN1 bus. May not enter normal mode. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| TXD1 | 1 | GND1 | CAN1 bus will enter dominant time out mode. Unable to transmit data to CAN1 bus. | B |
| GND1 | 2 | VCC | Device unpowered, high ICC current. | B |
| VCC | 3 | RXD1 | RXD1 output stuck high, unable to receive data from CAN1 bus. | B |
| RXD1 | 4 | GND2 | RXD default is high side FET ON, with pin short to ground, it forms direct path between supply and ground causing high current | A |
| GND2 | 5 | TXD2 | CAN2 bus will enter dominant time out mode. Unable to transmit data to CAN2 bus. | B |
| TXD2 | 6 | RXD2 | RXD2 output reflects the input to TXD2, and while this is the same transceiver, due to loop delay, the communication will be corrupted. Information from CAN2 bus will not be received correctly. | B |
| STB2 | 8 | CANL2 | CAN2 driver and receiver may turn off when the CAN2 bus is recessive. May not enter normal mode. | B |
| CANL2 | 9 | CANH2 | CAN2 bus stuck recessive, no communication possible. IOS current may be reached. | B |
| CANH2 | 10 | VIO | CAN2 bus stuck dominant, no communication possible. | B |
| VIO | 11 | CANL1 | CAN1 bus stuck recessive, no communication possible. IOS current may be reached on CANL1. | B |
| CANL1 | 12 | CANH1 | CAN1 bus stuck recessive, no communication possible IOS current may be reached. | B |
| CANH1 | 13 | STB1 | CAN1 driver and receiver turn off when a dominant is driven. May not enter normal mode. | B |
| Pin Name | Pin No. (TCAN1046A-Q1) | Pin No. (TCAN1046AV-Q1) | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| TXD1 | 1 | 1 | TXD1 pin stuck high, unable to transmit data to CAN1 bus. | B |
| GND1 | 2 | 2 | CAN1 transceiver unpowered, high ICC current. | B |
| VCC1 | 3 | - | None | D |
| VCC | - | 3 | None | D |
| RXD1 | 4 | 4 | RXD1 pin stuck high, unable to receive data from CAN1 bus. | B |
| TXD2 | 5 | 6 | TXD2 pin stuck high, unable to transmit data to CAN2 bus. | B |
| GND2 | 6 | 5 | CAN2 transceiver unpowered, high ICC current. | B |
| VCC2 | 7 | - | None | D |
| RXD2 | 8 | 7 | RXD2 pin stuck high, unable to receive data for CAN2 bus. | B |
| CANL2 | 9 | 9 | CAN2 bus always recessive, no communication possible. IOS current may be reached. | B |
| CANH2 | 10 | 10 | VO(REC) spec violated, degraded EMC performance on CAN2 bus. | C |
| STB2 | 11 | 8 | STB2 stuck high, CAN2 transceiver always in standby mode. | B |
| VIO | - | 11 | IO pins will operate as 5V input/output. Microcontroller may be damaged if VCC > VIO. | C |
| CANL1 | 12 | 12 | CAN1 bus always recessive, no communication possible. IOS current may be reached. | B |
| CANH1 | 13 | 13 | VO(REC) spec violated, degraded EMC performance on CAN1 bus. | C |
| STB1 | 14 | 14 | STB1 stuck high, CAN1 transceiver always in standby mode. |
| Pin Name | Pin No. (TCAN1046AV-Q1) | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| TXD1 | 1 | TXD1 stuck high, unable to transmit data to CAN1 bus. | B |
| GND1 | 2 | CAN1 unpowered, high IIO current. | B |
| VCC | 3 | IO pins will operate as 5V input/output. Microcontroller may be damaged if VCC > VIO. | C |
| RXD1 | 4 | RXD1 pin stuck high, unable to receive data from CAN1 bus. | B |
| GND2 | 5 | CAN2 unpowered, high IIO current. | B |
| TXD2 | 6 | TXD2 stuck high, unable to transmit data to CAN2 bus. | B |
| RXD2 | 7 | RXD2 pin stuck high, unable to receive data from CAN2 bus. | B |
| STB2 | 8 | STB2 stuck high, CAN2 transceiver always in standby mode. | B |
| CANL2 | 9 | CAN2 bus always recessive, no communication possible. IOS current may be reached if VIO ≥ 3.3V. | B |
| CANH2 | 10 | VO(REC) spec violated if VIO ≥ 3.3V, degraded EMC performance on CAN2 bus. | C |
| VIO | 11 | None | D |
| CANL1 | 12 | CAN1 bus always recessive, no communication possible. IOS current may be reached if VIO ≥ 3.3V. | B |
| CANH1 | 13 | VO(REC) spec violated if VIO ≥ 3.3V, degraded EMC performance on CAN1 bus. | C |
| STB1 | 14 | STB1 stuck high, CAN1 transceiver always in standby mode. | B |
| Pin Name | Pin No. (TCAN1046A-Q1) | Pin No. (TCAN1046AV-Q1) | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| TXD1 | 1 | 1 | Absolute maximum violation, transceiver may be damaged. Unable to transmit data to CAN1 bus. | A |
| GND1 | 2 | 2 | Device unpowered, high IBAT current. | B |
| VCC1 | 3 | - | Absolute maximum violation, transceiver may be damaged. CAN1 bus may be unable to communicate. | A |
| VCC | - | 3 | Absolute maximum violation, transceiver may be damaged. CAN bus may be unable to communicate. | A |
| RXD1 | 4 | 4 | Absolute maximum violation, transceiver may be damaged. Unable to receive data from CAN1 bus. | A |
| TXD2 | 5 | 6 | Absolute maximum violation, transceiver may be damaged. Unable to transmit data to CAN2 bus. | A |
| GND2 | 6 | 5 | Device unpowered, high IBAT current. | B |
| VCC2 | 7 | - | Absolute maximum violation, transceiver may be damaged. CAN2 bus may be unable to communicate. | A |
| RXD2 | 8 | 7 | Absolute maximum violation, transceiver may be damaged. Unable to receive data from CAN2 bus. | B |
| CANL2 | 9 | 9 | CAN2 bus always recessive, no communication possible. IOS current may be reached. | B |
| CANH2 | 10 | 10 | VO(REC) spec violated, degraded EMC performance on CAN2 bus. | C |
| STB2 | 11 | 8 | Absolute maximum violation, transceiver may be damaged. CAN2 transceiver stuck in standby mode. | A |
| VIO | - | 11 | Absolute maximum violation, transceiver may be damaged. | A |
| CANL1 | 12 | 12 | CAN1 bus always recessive, no communication possible. IOS current may be reached. | B |
| CANH1 | 13 | 13 | VO(REC) spec violated, degraded EMC performance on CAN1 bus. | B |
| STB1 | 14 | 14 | Absolute maximum violation, transceiver may be damaged. CAN1 transceiver stuck in standby mode. | A |